S32K146 LPO clock source select

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K146 LPO clock source select

ソリューションへジャンプ
2,050件の閲覧回数
ZhaozhangChen
Contributor I

Hi

    I use the default LPO clock 128Khz in the BootLoader, but I need to use LPO clock 1Khz in the APP, but when I set LPO clock 1Khz when the BootLoader jumps to the APP, it does not take effect.The value of LPOCLKSEL register is 00b. Is there any way to set LPO to 1KHz in app.

ZhaozhangChen_0-1665219450690.pngZhaozhangChen_1-1665219497269.png

 

0 件の賞賛
返信
1 解決策
2,040件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

Hi@ZhaozhangChen

The LPOCLKS register is a write-once register, and is reset only on POR or LVD.

 

please refer to S32K-RM,the chapter 11.3.1.4

Senlent_0-1665281155921.png

BR!

 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,041件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

Hi@ZhaozhangChen

The LPOCLKS register is a write-once register, and is reset only on POR or LVD.

 

please refer to S32K-RM,the chapter 11.3.1.4

Senlent_0-1665281155921.png

BR!

 

0 件の賞賛
返信