Hi@csava
Regarding the demo "adc_hwtrigger_s32k146",I made a test on S32K146EVB, and it works fine on my side.

Then test "adc_swtrigger_s32k146",

Both examples work well on S32K146EVB, so I'm pretty sure there should be no problem with these two routines, may be you can try check if the code has been modified or other reasons.
Those tests based on :
SDK: S32K1xx RTM SDK 3.0.0
IDE: S32K Design Studio for ARM 2018.R1
Hardware:S32K146EVB
BR!
Jim,
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------