S32K144 bootloader

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K144 bootloader

1,702 Views
vinaykl
Contributor III

Hello team,

     I have 2 S32K144 EVB's, I want to perform firmware update using bootloader via CAN FD interface. But as per the document given for bootloader "AN12323", we have to create one memory partition application, one bootloader application and one more gateway application. But I cannot find any of the example application in the latest SDK's. Please help. Thanks

Tags (1)
0 Kudos
Reply
3 Replies

1,638 Views
vinaykl
Contributor III

Hello @danielmartynek. Thanks for the reply. I am able to flash the custom binary created by me. But the bootloader couldn't able to boot the image what I have flashed. Will you please let me know how can I add the APPKEY in the project or linker file.

Thanks

0 Kudos
Reply

1,609 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Seems like this question has been already answered in your second thread on this issue:

https://community.nxp.com/t5/S32K/S32K144-bootloader/td-p/1716393

 

Regards,

Daniel

 

0 Kudos
Reply

1,663 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @vinaykl,

The AN comes with SW, but these are not SDK projects.

danielmartynek_0-1693833675274.png

 

There is Unified Bootloader:

https://community.nxp.com/t5/S32K-Knowledge-Base/Unified-bootloader-Demo/ta-p/1423099

 

Built in S32DS R1 IDE with SDK RTM 2.0.0

It was discussed in this thread:

https://community.nxp.com/t5/S32K/OTA-using-UDS-over-the-CAN/td-p/1640549

 

Regards,

Daniel

 

 

0 Kudos
Reply