S32K144 Watchdog timeout difference by 1 sec

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K144 Watchdog timeout difference by 1 sec

1,745件の閲覧回数
emb02
Contributor V

Hi,

I'm using S32K144 internal watchdog timer to reset controller. 

I'm using internal oscillator and Watchdog Clock source is WDOG_LPO_CLOCK = 128 KHz.

I'm using formula: timeout (s) = 256 * (1 / clk) * TOVAL

If Timeout = 1 sec then TOVAL = 500 but controller is resetting after 2 sec.

If Timeout = 3 sec then TOVAL = 1500 but controller is resetting after 4 sec.

If Timeout = 5 sec then TOVAL = 2500 but controller is resetting after 6 sec.

I'm getting difference of 1 sec always.

Clock settings:Clock.png

Watch Dog settings for 5 sec:

WDOG.png

Please help me with this.

0 件の賞賛
返信
1 返信

1,721件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @emb02,

 

The LPO clock is very imprecise, it is expected that 1s configured will not be exactly 1s.

danielmartynek_0-1692345933764.png

 

But in this case there is 1s offset regardless of the WDOG TOVAL.

 

The reset can be delayed by the WDOG interrupt (128 BUS_CLK cycles) and by the RCM interrupt (up to 512 LPO clock cycles).

https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K144-WDOG-RCM-interrupt/ta-p/1107039

 

I would say it must be an error of measurement, how exactly do you measure the timeout?

 

Regards,

Daniel

0 件の賞賛
返信