[S32K144][SCST] Hard Fault Test failure while checking a HFSR[FORCED] bit

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

[S32K144][SCST] Hard Fault Test failure while checking a HFSR[FORCED] bit

跳至解决方案
3,207 次查看
sunghou-kim
Contributor III

Hello, NXP team !

This is sungho.

I have an issue regarding using "core test solution(SCST)" for S32K144.

 

m4_scst_exception_hard_fault1 <= This test item not working fine so far.

 

On entry "m4_scst_ISR_dispatcher" , HFSR[FORCED]  is  set by illegal instruction. (plz see attached image)

sunghoukim_0-1626931846951.png

 

But soon as I proceed by one step(Trace32), It becomes clear....so test ends up with failure.(refer to an image below)

sunghoukim_1-1626931917887.png

sunghoukim_2-1626931991762.png

Would you mind giving me a hint for resolving this issue?

Thanks

Sungho

 

PS. I also tested it with demo app example(scst), but got failure with the same reason.

0 项奖励
回复
1 解答
3,190 次查看
martinkaspar-r3
NXP Employee
NXP Employee

Hello,

this is expected behavior because the FORCED flag is tied down by the debugger. Unfortunately, this feature complicates debugging of M4 SCST Library. The only possibility for debugging is to set the breakpoint just after the HFSR register is read.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
3,172 次查看
sunghou-kim
Contributor III

Thanks, martingkaspar-r3

I checked it working fine without Debugging attached.

Many thanks,

sunghou

0 项奖励
回复
3,191 次查看
martinkaspar-r3
NXP Employee
NXP Employee

Hello,

this is expected behavior because the FORCED flag is tied down by the debugger. Unfortunately, this feature complicates debugging of M4 SCST Library. The only possibility for debugging is to set the breakpoint just after the HFSR register is read.

0 项奖励
回复