S32K144   Pin_ What are the functions of the following statements in mux. h?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32K144   Pin_ What are the functions of the following statements in mux. h?

858 次查看
zhouqichen
Contributor I

S32K144   Pin_ What are the functions of the following statements in mux. h? Does deletion affect?

 

  PinSetting Configuration Generation Settings :
** UtilizeResetValuesCondGroup : Only if property present
** Generate configured Pins only : yes

0 项奖励
回复
1 回复

852 次查看
KalaimaniArumugamdev
Contributor III

Hi @zhouqichen,

"

Settings :  
 ** PinSetting Configuration Generation Settings :
 ** UtilizeResetValuesCondGroup : Only if property present
 ** Generate configured Pins only : yes
  

"

These comments are only used to inform you of the pin allocation based on the GUI.

You can delete these comments.

 

Thanks 

Kalaimani

0 项奖励
回复