S32K144 PCB Layout Guidelines

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K144 PCB Layout Guidelines

Jump to solution
2,966 Views
x112233
Contributor I

Hi,

I want to check the PCB design now, but I can't find any design guidelines in the specification.Can you provide me with the PCB design document for S32K144

thanks.

0 Kudos
Reply
1 Solution
2,934 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @x112233 

In the application note AN5426: Hardware Design Guidelines for S32K1xx are provided the General board layout guidelines in section 10. 

 

B.R.

VaneB

View solution in original post

0 Kudos
Reply
2 Replies
2,935 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @x112233 

In the application note AN5426: Hardware Design Guidelines for S32K1xx are provided the General board layout guidelines in section 10. 

 

B.R.

VaneB

0 Kudos
Reply
2,841 Views
AnhNguyenDuc
NXP Employee
NXP Employee

Hi @VaneB,

I want to measure the dimension between two headers on the board to make a adapter shield to connect with the board. Where can I find the these dimension ?

0 Kudos
Reply