S32K144 Debugging issues

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K144 Debugging issues

2,718 Views
Niupitang
Contributor III

The jlink in my hand is damaged, so I have to use PEmicro Mutlllink FX to debug... After referring to a large number of posts, the following problems always occur when entering debugging:Niupitang_0-1698741537983.pngNiupitang_0-1698741537983.png

The following is my debugging settings interface:

Niupitang_1-1698741583312.pngNiupitang_1-1698741583312.png

I hope someone can help solve this problem. The PE driver and hardware are normal. I have used it to debug MPC5748G. The wiring is also normal and the debugger yellow light lights up normally. TVCC has also been connected to the 5V of the development board.

 

 

0 Kudos
Reply
4 Replies

2,704 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

your Multilink FX debug probe is not recognized by system for some reason. Is the probe properly connected? Is visible in Windows Device manager? 

jiri_kral_0-1698747517987.pngjiri_kral_0-1698747517987.png

jiri_kral_1-1698747566225.pngjiri_kral_1-1698747566225.png

 

 

 

0 Kudos
Reply

2,662 Views
Niupitang
Contributor III
请问有什么解决方法吗
0 Kudos
Reply

2,635 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

you can try re-install PE Micro drivers. With default install path is driver located in c:\NXP\S32DS.3.5\Drivers\ folder. 

 

This issue is related to one particular S32K144 board or to all boards? 

0 Kudos
Reply

2,692 Views
Niupitang
Contributor III

Niupitang_0-1698801191894.pngNiupitang_0-1698801191894.png

Of course, I also used this debugger when I debug other processors.

 

0 Kudos
Reply