S32K144 DAC CMP0_out

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,635件の閲覧回数
dsilva
Contributor III

Hello,

I need an analog signal (0V to 10V) on pin 18 of the FS32K144 LQFP100 processor.

The configuration options for this pin are: FTM0_FLT0, LPUART2_RTS, FTM2_FLT0, TRGMUX_IN6 and CMP0_OUT.

Is it possible to use CMP0_OUT as an analog output?

0 件の賞賛
返信
1 解決策
2,624件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

The DAC from a comparator is available as an on-chip internal signal only and is not available externally to a pin.

45.2 Introduction.png45.2 Introduction.png

Figure 45-1. CMP high level diagram.pngFigure 45-1. CMP high level diagram.png
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,625件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

The DAC from a comparator is available as an on-chip internal signal only and is not available externally to a pin.

45.2 Introduction.png45.2 Introduction.png

Figure 45-1. CMP high level diagram.pngFigure 45-1. CMP high level diagram.png
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信