S32K144 DAC CMP0_out

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K144 DAC CMP0_out

Jump to solution
2,685 Views
dsilva
Contributor III

Hello,

I need an analog signal (0V to 10V) on pin 18 of the FS32K144 LQFP100 processor.

The configuration options for this pin are: FTM0_FLT0, LPUART2_RTS, FTM2_FLT0, TRGMUX_IN6 and CMP0_OUT.

Is it possible to use CMP0_OUT as an analog output?

0 Kudos
Reply
1 Solution
2,674 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

The DAC from a comparator is available as an on-chip internal signal only and is not available externally to a pin.

45.2 Introduction.png

Figure 45-1. CMP high level diagram.png
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
2,675 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

The DAC from a comparator is available as an on-chip internal signal only and is not available externally to a pin.

45.2 Introduction.png

Figure 45-1. CMP high level diagram.png
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply