S32K144 Can Callback Issue With Freertos TaskNotify

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K144 Can Callback Issue With Freertos TaskNotify

Jump to solution
2,661 Views
HarunCSaykal
Contributor II
   Hello
I work with S32K144 processor. I'm using Freertos. I'm using an interrupt for Can RX. When the RX interrupt occurs, I send a notify to a task. But when I send notify, I get stuck in the "portFORCE_INLINE static void vPortRaiseBASEPRI( void)" function.

    CAN_Init(&can_pal1_instance, &can_pal1_Config0);
    CAN_InstallEventCallback(&can_pal1_instance, CAN_TX_RX_Callback, NULL);

    can_recvtask_handle = xTaskCreateStatic(CAN_RecvTask,
                                            APP_CAN_RECV_TASK_NAME,
                                            APP_CAN_RECV_TASK_STACK,
                                            NULL,
                                            APP_CAN_RECV_TASK_PRIO,
                                            xRecvStack,          /* Array to use as the task's stack. */
                                            &xRecvTaskBuffer);

    
    void CAN_TX_RX_Callback(uint32_t instance, can_event_t eventType, uint32_t objIdx, void      *driverState)
    {
         /*check and handle the RX complete event*/
        if (CAN_EVENT_RX_COMPLETE == eventType) {
            CAN_Receive(&can_pal1_instance, objIdx, &rx_msg);
            BaseType_t xHigherPriorityTaskWoken = pdFALSE;
            xTaskNotifyFromISR(can_recvtask_handle, 0, eNoAction, &xHigherPriorityTaskWoken);  // The function that encounters the error.
            if (xHigherPriorityTaskWoken) {
                 portYIELD_FROM_ISR(xHigherPriorityTaskWoken);
            }
         }
      }


    static void CAN_RecvTask(void *Params)
   {
        (void)Params;
        while (pdTRUE) {
             xTaskNotifyWait(0, 0, eNoAction, portMAX_DELAY);
             J1939_Parser(rx_msg.id, &(rx_msg.data[0]));
        }
     }

xTaskNotifyFromISR(can_recvtask_handle, 0, eNoAction, &xHigherPriorityTaskWoken) is the function that falls into error.

I found out that this is an interrupt priority error. In another function, I was able to solve this problem by setting the interrupt priority.
http://www.FreeRTOS.org/RTOS-Cortex-M3-M4.html 

The code block below works without any issues.

#define LZ_PORT_IRQN        PORTD_IRQn
#define LZ_PORT_IRQN_PRI    (1)


app_status_t GPIO_install_int (void)

{
    /* Install LZ Button & INT interrupt handler */
    INT_SYS_InstallHandler(LZ_PORT_IRQN, RF_Instance_Int_Handler, (isr_t *)NULL);
    /* Enable LZ Button interrupt handler */
    INT_SYS_EnableIRQ(LZ_PORT_IRQN);

    INT_SYS_SetPriority(LZ_PORT_IRQN, LZ_PORT_IRQN_PRI);

    if (INT_SYS_GetPriority(LZ_PORT_IRQN) != LZ_PORT_IRQN_PRI) {
        return APP_STATUS_FAIL;
    }

    return APP_STATUS_OK;
}

void RF_Instance_Int_Handler (void)
{
    uint32_t u32Flags;

    u32Flags = GPIO_AML_GetInterruptFlags(SW_INT_LZ_INSTANCE);

    /* Check if interrupt comes from LZ INT pin */
    if (u32Flags & (1 << LZ_INT_PIN_NB)) {
        BaseType_t xHigherPriorityTaskWoken = pdFALSE;
        xTaskNotifyFromISR(RF_TaskHandle, 0, eNoAction, &xHigherPriorityTaskWoken);
        if (xHigherPriorityTaskWoken) {
            portYIELD_FROM_ISR(xHigherPriorityTaskWoken);
        }
        GPIO_AML_ClearInterruptFlags(SW_INT_LZ_INSTANCE, LZ_INT_PIN_NB);
    }
}


But I couldn't set this priority for Can interrupt. How can I set this priority for CAN RX, or what other solutions are there for this problem?
0 Kudos
Reply
1 Solution
2,620 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

you can set interrupt priority for given ISR in similar manner as for Port interrupt, using NT_SYS_SetPriority function. Just use right function parameters, like
INT_SYS_SetPriority(CAN0_ORed_0_15_MB_IRQn, 1);

BR, Petr

View solution in original post

0 Kudos
Reply
2 Replies
2,621 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

you can set interrupt priority for given ISR in similar manner as for Port interrupt, using NT_SYS_SetPriority function. Just use right function parameters, like
INT_SYS_SetPriority(CAN0_ORed_0_15_MB_IRQn, 1);

BR, Petr

0 Kudos
Reply
2,596 Views
HarunCSaykal
Contributor II

Solved. Yes, that's right fucn. Thank you.

0 Kudos
Reply