S32K144 CAN Remote request frames repeat sending all the time

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K144 CAN Remote request frames repeat sending all the time

5,553件の閲覧回数
paulzhou
Contributor II

Dear Sir 

   

   Use S32K144 SDK,S32K144 CAN moudle send standard frames and extended frames is No problem

   But when S32K144 CAN send Remote request frames , it's repeat sending all the time.

   Relative to the standard frame / extended frame, What's needs special attention for set S32K144 CAN remote frame?

   Do you have demo code for S32K144 CAN remote frame?

   Thank you

0 件の賞賛
返信
5 返答(返信)

5,234件の閲覧回数
felixfeng
Contributor I

Hi Paul,

     I try to establish to 10 ms task to send can messages. But it failed. The interval of frame monitored by PCan is not 10 ms in my expectation. It's disorder. What's the problem of my period task. Thanks.

0 件の賞賛
返信

5,234件の閲覧回数
AnaAldescu
NXP Employee
NXP Employee

Hello,

Could you please give us more details about your problem? Especially, I need to know if the Protocol Engine clock is sourced from the oscillator clock or the peripheral clock and which method did you choose for setting the CAN bitrate.

Thank you,

Ana

0 件の賞賛
返信

5,234件の閲覧回数
AnaAldescu
NXP Employee
NXP Employee

Hello,

There is indeed an issue with the S32 SDK FlexCAN driver for S32K144, which cannot respond to CAN Remote request frames. It will be fixed in the next release.

Regards,

Ana

0 件の賞賛
返信

5,234件の閲覧回数
paulzhou
Contributor II

Dear Ana

     Whether the latest version 0.86 of s32k144's SDK can support S32K144 CAN module to send remote frames?

Thank you

0 件の賞賛
返信

5,234件の閲覧回数
AnaAldescu
NXP Employee
NXP Employee

Hello Paul,

The FlexCAN driver from the EAR 0.8.6 SDK release has an issue with automatically responding to remote requests, but it is still able to send remote frames properly. This issue was fixed and it will be available in the upcoming BETA release.

Please let me know if I can assist you with this problem.

Best regards,

Ana

0 件の賞賛
返信