S32K144 Bootloader via CAN

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K144 Bootloader via CAN

6,965 Views
autics
Contributor III

Hello NXP,

My objective is to update S32K144 via CAN. 

I have S32K144 EVA, PE Multilink universal, S32 Design Studio for S32 Platform 3.4 and PCAN tool.

I've tried to study through the example link below, but I'm not sure how to approach it.

I've understood the concept of bootloaders.

How can I do it on the S32 Design Studio for S32 Platform ?

 https://community.nxp.com/t5/S32K/S32K-bootloader-over-CAN/m-p/1067266#:~:text=https%3A//www.nxp.com... 

Unified Bootloader -User Guide 

0 Kudos
Reply
13 Replies

6,708 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@autics

please create a ticket so that we can sent it to you.

https://support.nxp.com/s/?language=en_US

 

0 Kudos
Reply

6,946 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@autics

you can't directly run this demo "S32K144_CAN_bootloader" in S32 Design Studio for S32 Platform 3.4

it just because this demo run's on RTM 3.0.X and S32 DS V3.4 or V3.5 can't support this version.

So you can install S32 Design Studio for Arm or manually port this routine to the new IDE platform.

0 Kudos
Reply

6,942 Views
autics
Contributor III

Thank you for your quick response.

I just installed S32 Design Studio for ARM Version 2.2 

I'm really sorry, but what should I do next?

 

0 Kudos
Reply

6,934 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@autics

I suggest you to install S32 Design Studio For Arm  2018 and install the RTM below.

https://www.nxp.com/design/design-center/software/development-software/s32-design-studio-ide/s32-des...

Senlent_0-1705993503613.png

or you can try install it in V2,2, but i don't know if this have problem or not.

0 Kudos
Reply

6,918 Views
autics
Contributor III

I'm ready now.
I'd like to ask a realistic question first. Shouldn't I put the bootloader program on the S32K144 eVA board first?

I would appreciate it if you could support me with what files and how to put them in the bootloader.

I'm so frustrated, and I want to do a solution. I'm so sorry.

0 Kudos
Reply

6,899 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@autics

yes, you should download the Bootloader to MCU first with an debugger,

then use OpenBus Software through PCAN software to download flash driver and App to MCU.

0 Kudos
Reply

6,798 Views
autics
Contributor III

NXP1.png

I understood it as saying to compile and download the bootloader folder file of the above image.
Is that right?

However, there was an error in not finding several files as shown in the image below.
Explorer has confirmed the existence of a file. How should I connect you?

 

NXP.png

 

 

0 Kudos
Reply

6,771 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@autics

these two files you can find in the below path, you can add it to your project.

Senlent_0-1706495388235.png

 

0 Kudos
Reply

6,749 Views
autics
Contributor III

After clearing all the errors, I ran debug mode.

Blue LED blinks as shown in the image below. Is that correct?

제목 없음.png

0 Kudos
Reply

6,720 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@autics

if you can enter the debug page normally, it means there is no problem.

0 Kudos
Reply

6,712 Views
autics
Contributor III

I'm so sorry and thank you.

Where can I download  the NXP OpenBus Software ?

00593779

0 Kudos
Reply

6,690 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@autics

I see someone is already handling your case.
Please pay attention to your problem description next time. Why didn't you just say you wanted to apply for NxpOpenBus when you created a new case?

 

0 Kudos
Reply

6,666 Views
autics
Contributor III

제목 없음.png

There seems to be a misunderstanding.
I think it's because it's my first time using NXP Community.
Looking at other people's conversations, And I received the above email asking me to create a ticket. I think I need to get a unique number to receive NXP OpenBus Software, so I'm trying to get a number, so I think I'm having this problem.

I'm so sorry.

I really want to solve this problem.

Honestly, I don't even know what ticket creation is.
Can't you help me?

0 Kudos
Reply