S32K144 Bootloader via CAN

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32K144 Bootloader via CAN

6,943 次查看
autics
Contributor III

Hello NXP,

My objective is to update S32K144 via CAN. 

I have S32K144 EVA, PE Multilink universal, S32 Design Studio for S32 Platform 3.4 and PCAN tool.

I've tried to study through the example link below, but I'm not sure how to approach it.

I've understood the concept of bootloaders.

How can I do it on the S32 Design Studio for S32 Platform ?

 https://community.nxp.com/t5/S32K/S32K-bootloader-over-CAN/m-p/1067266#:~:text=https%3A//www.nxp.com... 

Unified Bootloader -User Guide 

0 项奖励
回复
13 回复数

6,686 次查看
Senlent
NXP TechSupport
NXP TechSupport

Hi@autics

please create a ticket so that we can sent it to you.

https://support.nxp.com/s/?language=en_US

 

0 项奖励
回复

6,924 次查看
Senlent
NXP TechSupport
NXP TechSupport

Hi@autics

you can't directly run this demo "S32K144_CAN_bootloader" in S32 Design Studio for S32 Platform 3.4

it just because this demo run's on RTM 3.0.X and S32 DS V3.4 or V3.5 can't support this version.

So you can install S32 Design Studio for Arm or manually port this routine to the new IDE platform.

0 项奖励
回复

6,920 次查看
autics
Contributor III

Thank you for your quick response.

I just installed S32 Design Studio for ARM Version 2.2 

I'm really sorry, but what should I do next?

 

0 项奖励
回复

6,912 次查看
Senlent
NXP TechSupport
NXP TechSupport

Hi@autics

I suggest you to install S32 Design Studio For Arm  2018 and install the RTM below.

https://www.nxp.com/design/design-center/software/development-software/s32-design-studio-ide/s32-des...

Senlent_0-1705993503613.png

or you can try install it in V2,2, but i don't know if this have problem or not.

0 项奖励
回复

6,896 次查看
autics
Contributor III

I'm ready now.
I'd like to ask a realistic question first. Shouldn't I put the bootloader program on the S32K144 eVA board first?

I would appreciate it if you could support me with what files and how to put them in the bootloader.

I'm so frustrated, and I want to do a solution. I'm so sorry.

0 项奖励
回复

6,877 次查看
Senlent
NXP TechSupport
NXP TechSupport

Hi@autics

yes, you should download the Bootloader to MCU first with an debugger,

then use OpenBus Software through PCAN software to download flash driver and App to MCU.

0 项奖励
回复

6,776 次查看
autics
Contributor III

NXP1.png

I understood it as saying to compile and download the bootloader folder file of the above image.
Is that right?

However, there was an error in not finding several files as shown in the image below.
Explorer has confirmed the existence of a file. How should I connect you?

 

NXP.png

 

 

0 项奖励
回复

6,749 次查看
Senlent
NXP TechSupport
NXP TechSupport

Hi@autics

these two files you can find in the below path, you can add it to your project.

Senlent_0-1706495388235.png

 

0 项奖励
回复

6,727 次查看
autics
Contributor III

After clearing all the errors, I ran debug mode.

Blue LED blinks as shown in the image below. Is that correct?

제목 없음.png

0 项奖励
回复

6,698 次查看
Senlent
NXP TechSupport
NXP TechSupport

Hi@autics

if you can enter the debug page normally, it means there is no problem.

0 项奖励
回复

6,690 次查看
autics
Contributor III

I'm so sorry and thank you.

Where can I download  the NXP OpenBus Software ?

00593779

0 项奖励
回复

6,668 次查看
Senlent
NXP TechSupport
NXP TechSupport

Hi@autics

I see someone is already handling your case.
Please pay attention to your problem description next time. Why didn't you just say you wanted to apply for NxpOpenBus when you created a new case?

 

0 项奖励
回复

6,644 次查看
autics
Contributor III

제목 없음.png

There seems to be a misunderstanding.
I think it's because it's my first time using NXP Community.
Looking at other people's conversations, And I received the above email asking me to create a ticket. I think I need to get a unique number to receive NXP OpenBus Software, so I'm trying to get a number, so I think I'm having this problem.

I'm so sorry.

I really want to solve this problem.

Honestly, I don't even know what ticket creation is.
Can't you help me?

0 项奖励
回复