S32K144 Bootloader via CAN

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K144 Bootloader via CAN

7,007件の閲覧回数
autics
Contributor III

Hello NXP,

My objective is to update S32K144 via CAN. 

I have S32K144 EVA, PE Multilink universal, S32 Design Studio for S32 Platform 3.4 and PCAN tool.

I've tried to study through the example link below, but I'm not sure how to approach it.

I've understood the concept of bootloaders.

How can I do it on the S32 Design Studio for S32 Platform ?

 https://community.nxp.com/t5/S32K/S32K-bootloader-over-CAN/m-p/1067266#:~:text=https%3A//www.nxp.com... 

Unified Bootloader -User Guide 

0 件の賞賛
返信
13 返答(返信)

6,750件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

Hi@autics

please create a ticket so that we can sent it to you.

https://support.nxp.com/s/?language=en_US

 

0 件の賞賛
返信

6,988件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

Hi@autics

you can't directly run this demo "S32K144_CAN_bootloader" in S32 Design Studio for S32 Platform 3.4

it just because this demo run's on RTM 3.0.X and S32 DS V3.4 or V3.5 can't support this version.

So you can install S32 Design Studio for Arm or manually port this routine to the new IDE platform.

0 件の賞賛
返信

6,984件の閲覧回数
autics
Contributor III

Thank you for your quick response.

I just installed S32 Design Studio for ARM Version 2.2 

I'm really sorry, but what should I do next?

 

0 件の賞賛
返信

6,976件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

Hi@autics

I suggest you to install S32 Design Studio For Arm  2018 and install the RTM below.

https://www.nxp.com/design/design-center/software/development-software/s32-design-studio-ide/s32-des...

Senlent_0-1705993503613.png

or you can try install it in V2,2, but i don't know if this have problem or not.

0 件の賞賛
返信

6,960件の閲覧回数
autics
Contributor III

I'm ready now.
I'd like to ask a realistic question first. Shouldn't I put the bootloader program on the S32K144 eVA board first?

I would appreciate it if you could support me with what files and how to put them in the bootloader.

I'm so frustrated, and I want to do a solution. I'm so sorry.

0 件の賞賛
返信

6,941件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

Hi@autics

yes, you should download the Bootloader to MCU first with an debugger,

then use OpenBus Software through PCAN software to download flash driver and App to MCU.

0 件の賞賛
返信

6,840件の閲覧回数
autics
Contributor III

NXP1.png

I understood it as saying to compile and download the bootloader folder file of the above image.
Is that right?

However, there was an error in not finding several files as shown in the image below.
Explorer has confirmed the existence of a file. How should I connect you?

 

NXP.png

 

 

0 件の賞賛
返信

6,813件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

Hi@autics

these two files you can find in the below path, you can add it to your project.

Senlent_0-1706495388235.png

 

0 件の賞賛
返信

6,791件の閲覧回数
autics
Contributor III

After clearing all the errors, I ran debug mode.

Blue LED blinks as shown in the image below. Is that correct?

제목 없음.png

0 件の賞賛
返信

6,762件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

Hi@autics

if you can enter the debug page normally, it means there is no problem.

0 件の賞賛
返信

6,754件の閲覧回数
autics
Contributor III

I'm so sorry and thank you.

Where can I download  the NXP OpenBus Software ?

00593779

0 件の賞賛
返信

6,732件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

Hi@autics

I see someone is already handling your case.
Please pay attention to your problem description next time. Why didn't you just say you wanted to apply for NxpOpenBus when you created a new case?

 

0 件の賞賛
返信

6,708件の閲覧回数
autics
Contributor III

제목 없음.png

There seems to be a misunderstanding.
I think it's because it's my first time using NXP Community.
Looking at other people's conversations, And I received the above email asking me to create a ticket. I think I need to get a unique number to receive NXP OpenBus Software, so I'm trying to get a number, so I think I'm having this problem.

I'm so sorry.

I really want to solve this problem.

Honestly, I don't even know what ticket creation is.
Can't you help me?

0 件の賞賛
返信