S32K144 AMMCLIB MLIB_Div_F32() Precision Problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K144 AMMCLIB MLIB_Div_F32() Precision Problem

2,799件の閲覧回数
420113461
Contributor I

When using ammclib tool library for division calculation, the last 15 bit(bit14 --- bit0) results of each calculation are 0, and the actual accuracy is only 16 bit(bit30 --- bit15).

code.pngcode.pngdebug.pngdebug.png

0 件の賞賛
返信
4 返答(返信)

2,597件の閲覧回数
petrz_
NXP Employee
NXP Employee

Hi,

we added a new library function MLIB_DivSatAccurate_F32 in the AMMCLib release 1.1.26. This function calculates the division with full 32-bit accuracy of the result. The function is faster than 64-bit by 32-bit division (if you relied on compiler's optimization capabilities) but not as fast as MLIB_DivSat_F32.

0 件の賞賛
返信

2,794件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

I can see it corresponds to the description. There's a note:

lukaszadrapa_0-1599544210237.pnglukaszadrapa_0-1599544210237.png

 

Regards,

Lukas

 

0 件の賞賛
返信

2,788件の閲覧回数
420113461
Contributor I

What's the difference between the three versions of ammclib library? Will it improve the calculation accuracy?AMMCLIB.pngAMMCLIB.png

0 件の賞賛
返信

2,780件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

There's no difference. It just means if you have want to get object code for evaluation or if you want to buy a license for production (either object code only or full source code).

Regards,

Lukas

 

0 件の賞賛
返信