S32K144 ADC Software Trigger

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K144 ADC Software Trigger

1,941 Views
raviranjankumar
Contributor III

Hi,

I am working on S32K144 ADC driver. In this, software trigger is only available for SC1A. If I want to use more than one channel with software trigger then how I can read the result. 

Please Help.

Thanks and regard,

Ravi Ranjan

0 Kudos
Reply
3 Replies

1,415 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi Ravi,

You can refer to the following threads.

https://community.nxp.com/message/867719

https://community.nxp.com/message/851097

 

BR, Petr

0 Kudos
Reply

1,415 Views
raviranjankumar
Contributor III

Hi Petr,

Now it is working fine in back to back mode but if I want to configure more than 8 channels then how and  I am not able to configure independent single channel except channel 0 (SC1A). 

Please help.

Thanks and Regard,

Ravi Ranjan

0 Kudos
Reply

1,415 Views
raviranjankumar
Contributor III

Hi Petr,

Thank you. It's really helpful for me.

0 Kudos
Reply