S32K142 RAM Allocation

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32K142 RAM Allocation

3,624 次查看
bjrajendra
Senior Contributor I

Hello all,

I'm using S32K142 device and implementing the following.

Basically I'm passing 32-byte array and sending those via can. But I observed that the data changed during the variable got changed during the process & understood that there might be an issue with the memory allocation.

I observed that the device has two sections and allocates data. I used the default setting.

Kindly suggest How to allocate into the both RAM sections.

Raju 

标签 (1)
0 项奖励
回复
3 回复数

3,537 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

unfortunately I do not fully understand the question and the issue.

If you deals with filling message buffer data words then you can refer to 

Transmit FlexCAN S32K148 

If you want to have bigger payload in the CAN message (8 byte by default) then CAN FD feature have to be enabled and you need to choose payload size for message buffers using FDCTRL[MBDSRn] bit fields. Note for higher payloads the MBs address offset varies.

Refer to chapters 55.4.4 FlexCAN memory partition for CAN FD and 55.4.5 FlexCAN message buffer memory map of the RM.

BR, Petr

0 项奖励
回复

3,537 次查看
bjrajendra
Senior Contributor I

Hi Petr,

Thanks for the response.

In fact, I'm passing a 32byte array over a pointer using a function as shown below.

void shareInfo(uint8_t *f_data)

Here the pointer f_data points to an 32-byte array. But during the transfer of the 32-byte data the array is getting modified because of the other function variables.

Kindly suggest some alternatives.

Raju

0 项奖励
回复

3,537 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

I'am afraid that without more explanation, code or project I am not able to suggest more.

BR, Petr

0 项奖励
回复