S32K118 Interrupts

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K118 Interrupts

1,665 Views
paolonese
Contributor I

Hi all,

I am triyng to setup an interrupt on LPTI timer or LPTMR0 one.

Both timers are running in the correct way (the end count flags will be settled) but

no way to get the interrupt.

I am using S32K118 evaluation board and S32DS IDE.

Can someone help me?

Thanks in advance.

0 Kudos
Reply
2 Replies

300 Views
dadin852
Contributor I

You can also get the interrupt examples through installing "S32SDK_S32K1xx_RTM_4.0.2.exe"

0 Kudos
Reply

1,642 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Please refer to the LPIT and LPTMR interrupt examples in S32K1 SDK 4.0.3 of S32DS v3.4.

lpit lptmr interrupt S32K1 SDK RTM 4.0.3.png


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------