Hi all,
I am triyng to setup an interrupt on LPTI timer or LPTMR0 one.
Both timers are running in the correct way (the end count flags will be settled) but
no way to get the interrupt.
I am using S32K118 evaluation board and S32DS IDE.
Can someone help me?
Thanks in advance.
Hi
Please refer to the LPIT and LPTMR interrupt examples in S32K1 SDK 4.0.3 of S32DS v3.4.
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------