S32K116EVB-Q048 RGB LED not working

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K116EVB-Q048 RGB LED not working

Jump to solution
5,810 Views
NicoloStrozzi
Contributor III

Hi, 

I've just started using the S32K116EVB-Q048 for a prototype development, starting from the basic examples in order to verify the PINout.

I've tried to run the "S32K116_Project_hello" and the "ftm_combined_pwm_s32k116" projects. Both are correctly compiled and loaded on the board, but I'm not able to make the RGB LED work. The LED is fine, I've checked with external power supply.

It seems that the issue is related to the J109, J110 and J111 headers, but I'm not able to find the correct documentation about these headers because all the docs on the NXP website is related to the previous EVB version.

Some suggestion on how to make the example projects work and turn on the LED?

0 Kudos
Reply
1 Solution
5,762 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Thank you for the report!
Sorry for the inconvenience we bring you!

It was an assembly error/issue. I will be escalating this case with the warehouse and Boards solution team to review all boards in stock.

I would recommend fixing the EVB with a local NXP team.

View solution in original post

3 Replies
5,798 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi NicoloStrozzi,

Seems that you are using S32K116EVB2Q048 instead of S32K116EVB-Q048.
Please download the Schematics of S32K116EVB2Q048 Evaluation Board.
The default jumper setting of J109 J110 J111 is not connect MCU pins to LED. In order to use these LEDs, you need to change the jumper setting .

J109 J110 J111 S32K116EVB2Q048.pngJ109 J110 J111 S32K116EVB2Q048.png

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

5,786 Views
NicoloStrozzi
Contributor III

Hi @Robin_Shen,

 

thank you very much for the quick reply and for the schematics, I haven't found them on the website.

We have tested all the connection to the LED with a tester, and it seems to us that in our board the LED is mounted upside down

I attach a couple of pics to this thread, could you please let me know if it's so?

 

0 Kudos
Reply
5,763 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Thank you for the report!
Sorry for the inconvenience we bring you!

It was an assembly error/issue. I will be escalating this case with the warehouse and Boards solution team to review all boards in stock.

I would recommend fixing the EVB with a local NXP team.