S32K116 CAN Receive

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K116 CAN Receive

1,395件の閲覧回数
tklauke
Contributor I

I use CAN in the S32K116. Sending and receiving works so far. Now I would like to use the option to store a callback to receive. So how do I use CAN_InstallEventCallback?

0 件の賞賛
返信
1 返信

1,366件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Please refer to the examples in S32K1xx SDK FlexCAN sample projects to demonstrate its basic and advanced features.

Here you will see how to use CAN_InstallEventCallback in S32K144_CAN_PAL_SamplePrj_Basic_TxRx_ID_FiltersConfig_SDKRTM3P0:

CAN_InstallEventCallback.png


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信