S32K148EVB - Not able to connect, Reset LED always on

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K148EVB - Not able to connect, Reset LED always on

589 Views
luk90as
NXP Employee
NXP Employee

I am not able to connect to the S32K148 board via OpenSDA USB using S32DS v2.2 for ARM. The Board shows on the explorer and also on the device manager. The used port is automatically recognized in the debug configuration in S32DS. The Reset LED D11 is always on. 

I tried to recover the board using kinetis Recovery Utility, but it was unable to halt the processor. I used the OpenSDA interface via USB.

0 Kudos
Reply
2 Replies

392 Views
eshivashankar
Contributor I

same issue for me also...D11 is always on...

 

0 Kudos
Reply

580 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi Lukas,

What error message do you get from the debugger?

 

BR, Daniel

0 Kudos
Reply