S32K116 CAN RX for FIFO mode----data coverage

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K116 CAN RX for FIFO mode----data coverage

3,024件の閲覧回数
jia_zw
Contributor I

Why is there still data coverage  , use  CAN RX  for FIFO mode ??

The phenomenon is as follows:

         send can a message  every 100 ms微信截图_20190408103600.png

タグ(1)
0 件の賞賛
返信
4 返答(返信)

2,802件の閲覧回数
jia_zw
Contributor I

hi Petr Stancik,

      As follows:i want to develop CAN bootloader for update;

                 1.   data_temp array    is used for update  PFlash data;

                               is from CAN interrupt         

                 2.  CAN FIFO mode config:

                      a. CAN init  & CAN Filter config

                                微信截图_20190415092534.png

                  

                             I close CAN FD

                          微信截图_20190415093206.png

   

                      b. start CAN recevie

                    微信截图_20190415092701.png

                    

                     c.intterupt

                     微信截图_20190415092747.png

                     

                  3. send  CAN message

                  I send  one CAN mesage  every 100 ms  through  CAN tools,

                  but  the  data_temp array  for recevie data   is  different form   the data   i  send

           Can you help  me  analyze  the question ?    thanks

0 件の賞賛
返信

2,802件の閲覧回数
jia_zw
Contributor I

hi,

     for example: 

 微信截图_20190415145033.png

0 件の賞賛
返信

2,802件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

it seems the received yellow marked bytes are the one from address 50h of the srec file.

This may point you lost some frames. Do you call CanStartRecv() fast enough so RXFIFO can be read out? Should be called each time callback is executed.

BR, Petr  

0 件の賞賛
返信

2,802件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

could you please describe the issue in more detail? How is the CAN used in your case?

What is data_temp array used for? Do you use any kind of demo example? 

BR, Petr

0 件の賞賛
返信