S32K1 ISELED R21-11 0.9.0 CD01 example project

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

S32K1 ISELED R21-11 0.9.0 CD01 example project

跳至解决方案
12,493 次查看
6T9
Contributor III

Hello,

I'm trying to explore an ILaS example project.

I created a new S32DS project form Example (S32K1 ISELED AUTOSAR R21-11 0.9.0 CD01 D2403 Example Project -> Iseled_FlexIO_example_S32K144_DS)
The newly created project is shown in the project explorer.

When I try to open the Iseled_example_DS.mex file I get an error.

Error during opending configuration Iseled_example_DS.mex:

Processor S32K144, the PlatformSDK_S32K1_S32M24 version is not supported by the current version of the tool.

Am I missing some files which must be installed?

Best regards

标记 (1)
0 项奖励
回复
1 解答
12,176 次查看
6T9
Contributor III

Hi Robin,

thanks for your support.

I have reinstalled everything, step by step. But the error still appeared.

I finally found the issue.

After reinstalling SW32K1_S32M24X_RTD_4.4_R21-11_2.0.0_D2308_DS_Updatesite.zip with the offline package it worked. I assume something went wrong during installation of this package.

Now I can open the .mex files.

 

Best regards

在原帖中查看解决方案

0 项奖励
回复
11 回复数
12,462 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Sorry, I did not find S32K1 ISELED AUTOSAR R21-11 0.9.0 CD01 D2403 on the Automotive SW - ISELED Software page. If it is convenient, please tell me where to download it.

Usually the Release Note will prompt which software it depends on. For example, SW32K1_ISELED_4.4_0.8.0_ReleaseNotes.pdf mentioned: This is the S32K1 ISELED AUTOSAR 4.4 Version 0.8.0 release containing ISELED driver on top of S32K1 RTD AUTOSAR 4.4 Version 1.0.1.
So we need to install S32K1 RTD 1.0.1 in S32DS first. Does the release note of S32K1 ISELED R21-11 0.9.0 CD01 mention which version of S32K1 RTD needs to be installed? Have you completed the installation of this version of S32K1 RTD?


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复
12,459 次查看
6T9
Contributor III

Hi,

I have downloaded it from the ISELED Software Page

6T9_0-1710917697414.png

 

I attached the release notes. The installation instruction mention the following:

SW32K1_ISELED_R21-11_0.9.0_ CD01_D2403_DS_updatesite.zip on top of
SW32K1_S32M24X_RTD_4.4_R21-11_2.0.0_D2308_DS_updatesite.zip

The RTD update site SW32K1_S32M24X_RTD_4.4_R21-
11_2.0.0_D2308_DS_updatesite.zip and SW32K1_ISELED_R21-11_0.9.0_
CD01_D2403_DS_updatesite.zip for S32 Design Studio should be installed by using the
Help -> Install New Software mechanism.

I can not find SW32K1_S32M24X_RTD_4.4_R21-11_2.0.0_D2308_DS_updatesite.zip. Where can I download this package?

 

Best regards

Thomas

0 项奖励
回复
12,456 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Real-Time Drivers for S32K1 -> Automotive SW - S32K1_S32M24x - Real-Time Drivers for Cortex-M -> S32K1_S32M24X Real Time Drivers AUTOSAR 4.4 & R21-11 Version 2.0.0

Refer to Offline Package Installation Setup of S32DS Extensions & Updates: Explanation and How To Use

0 项奖励
回复
12,453 次查看
6T9
Contributor III

Thanks for the package.
I tried to delete the example projects and create them again.

I tried the ISELED examples within in the AUTOSAR folder and the folder below.

6T9_0-1710924025191.png

Unfortunately I'm getting the same error after trying to open the .mex file for each example project.

6T9_1-1710924160605.png

Still the same error as before.

How can I solve this?

0 项奖励
回复
12,379 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Error during opending configuration Iseled_example_DS.mex: Processor S32K144, the PlatformSDK_S32K1_S32M24 version is not supported by the current version of the tool. This type of error is usually caused by not installing the S32DS Update mentioned in the S32K RTD release note.

Did you install S32K1 RTD by follow Offline Package Installation Setup of S32DS Extensions & Updates: Explanation and How To Use ?

According to the chapter '1.2.2 Delivered as an extension for S32 Design Studio' of SW32K1_S32M24x_RTD_4.4_R21-11_2.0.0_D2308_ReleaseNotes.pdf: You need to install "S32DS 3.5 Update 4 for S32K1", that is, step 2. Install Update 4 for S32DS: com.nxp.s32ds.update_3.5.4.20230707034206.zip

install S32DS 3.5 Update 4 for S32K1  SW32K1_S32M24x_RTD_4.4_R21-11_2.0.0_D2308_ReleaseNotes.png
Is it strange that the Offline Package Installation method does not automatically install "S32DS 3.5 Update 4 for S32K1" for your S32DS?
Then I'm afraid you need to install it manually, please download S32 Design Studio 3.5 Update 4 D2307 from the S32 Design Studio for S32 Platform web page and install it offline.

0 项奖励
回复
12,364 次查看
6T9
Contributor III

It is not possible to install update 4, because my current version (update 10) is higher than the one which shall be installed.

6T9_0-1711001172138.png

 

0 项奖励
回复
12,361 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Try uninstall Update 10, and then install Update 4.
Help -> Installation Details -> Uninstall... S32 Design Studio and S32 Design Studio Tools.

0 项奖励
回复
12,354 次查看
6T9
Contributor III

I have uninstalled S32DS 3.5 and started from scratch.

I executed the following steps:

  1. Installed S32DS 3.5
  2. Installed S32DS 3.5 Update 4
    6T9_1-1711013220124.png
  3. Installed S32K1_S32M24X Real Time Drivers AUTOSAR 4.4 & R21-11 Version 2.0.0
  4. Installed SW32K1_ISELED_R21-11_0.9.0_ CD01_D2403_DS_updatesite.zip

 

I still can not open the .mex file

6T9_2-1711013363065.png

 

Afterwards I installed update 10 again, but the error stays.

 

0 项奖励
回复
12,270 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

I uninstalled S32DS and reinstalled it this morning. It's strange that the reminder I encountered is different from your error.

Loaded configuration has been created by newer version of the tool. If saved, some information may be lost.png

Even though S32DS extensions and Updates offline install S32K1S32M24X Real Time Drivers AUTOSAR 4.4&R21-11 Version 2.0.0 and SW32K1-ISELEID-R21-11:0.9.0_ CD01-D2403/DS-updatesite.zip did not automatically install S32DS Update 4 or 10.
Even so, I can still open the. mex file without any errors.

S32DS Extensions and Updates offline install S32K1 RTD 2.0.0.pngS32DS Extensions and Updates install S32K1 RTD and development package.pngS32DS Extensions and Updates install confirm.png

Here is the Installation Details after finish installed S32K1S32M24X Real Time Drivers AUTOSAR 4.4&R21-11 Version 2.0.0:

Installation Details after offline install S32K1 RTD 2.0.0.png

 

Using the same method, install SW32K1-ISELEID-R21-11:0.9.0_ CD01-D2403/DS updatesite.zip.

Here is the Installation Details after finish installed SW32K1-ISELEID-R21-11:0.9.0_ CD01-D2403/DS updatesite.zip:

Installation Details after offline install S32K1 ISELED AUTOSAR R21-11 0.9.0 CD01.png

I am able to open .mex file. 

Iseled_FlexIO_example_S32K144_DS S32CT.png

0 项奖励
回复
12,177 次查看
6T9
Contributor III

Hi Robin,

thanks for your support.

I have reinstalled everything, step by step. But the error still appeared.

I finally found the issue.

After reinstalling SW32K1_S32M24X_RTD_4.4_R21-11_2.0.0_D2308_DS_Updatesite.zip with the offline package it worked. I assume something went wrong during installation of this package.

Now I can open the .mex files.

 

Best regards

0 项奖励
回复
12,484 次查看
6T9
Contributor III

6T9_0-1710764363029.png

S32DS Version

 

0 项奖励
回复