S32K QSPI

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K QSPI

3,619 Views
wanglijun
Contributor II

Dears,

I have a question about S32K148 QSPI:

I configured the QSPI clock, but I measured using the oscilloprobe, it is noise wave.

Any point need to be cared?

 

Thank you!

0 Kudos
Reply
4 Replies

3,601 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi wanglijun,

Have you refer the qspi_external_flash_s32k148 in S32SDK S32K1xx RTM v3.0.0 Example Projects?

qspi_external_flash_s32k148.png

If you are using S32K148EVB, are you measure the QSPI_A_SCK at pin6 of U508?

U508 S32K148EVB.jpg
Have you change the hardware according to the description of External Flash over QuadSPI?

Robin_Shen_0-1630564999615.png

Can you describe the configuration in detail? Maybe you can screenshot your configuration of clock and QSPI.

Best Regards,
Robin

0 Kudos
Reply

3,571 Views
wanglijun
Contributor II

Hello,

I am not using the EVB, but the configuration is same with the example.

If the external flash is same with the EVB, and the external flash requires 3.3V.

If the MCU is 5V, is it OK in CLK signal?

0 Kudos
Reply

3,565 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

I am afraid you can't connect 5V signal to MX25L6433FM2R-08G.

MX25L6433FM2R-08G.png

Have you tested whether it can communicate through QSPI under the condition of 3.3V power supply S32K148? 

Or refer to S32K148EVB to use Bidirectional Voltage-Level Translator.

0 Kudos
Reply

3,554 Views
wanglijun
Contributor II

ok.

Additionally, is there special note about the QSPI initialization?

Thank you!

0 Kudos
Reply