S32K ECC functionality

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K ECC functionality

ソリューションへジャンプ
6,923件の閲覧回数
andals
Contributor I

We are trying to understand which memory types of the S32K is protected by ECC. It is clear from the S32K1xx Series Reference Manual that both sections of RAM is protected as well as how to detect both single-bit and double-bit ECC errors. For the FlexNVM module it is also clear that if it is configured as Data Flash or Emulated EEPROM, single-bit ECC errors are automatically corrected and how to detect double-bit ECC errors. If CSEc is used, it is also clear that CSE_PRAM area is protected.

However, for the regular data/program flash (ex in S32K148 address range: 0000_0000-0017_FFFF ), it is not clear for us from the Reference Manual or other S32K documentation if it is ECC protected and how. It seems like double-bit faults in regular flash is reported in register FTFC->FERSTAT->DFDIF (Double Bit Fault Detect Interrupt Flag). Is this correct? For single-bit faults in regular flash there is less information:  Is it in place for regular flash? Is it automatically corrected? Is there any reporting of it?

Best regards,

André

0 件の賞賛
返信
1 解決策
6,871件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

That's a good point, you are right. Sorry, I mismatched that with another devices where it is possible.

I just confirmed that there's no flag for single bit error. Only double bit error can be reported on flash.

Regards,

Lukas

 

元の投稿で解決策を見る

0 件の賞賛
返信
8 返答(返信)
1,410件の閲覧回数
durga_choudhury
Contributor IV

I have a few related questions on this topic:

1. Is there a way, either in software or hardware, to 'scrub' memory that needs ECC correction? ('scrubbing' means writing back the correct value to the memory location so it won't need ECC correction next time).

2. In case of double bit errors, how is this reported? Does the user application need to read the register mentioned in this discussion or is there some asynchronous (e.g. interrupt) method also exists?

 

Thanks for your help

Durga Choudhury

0 件の賞賛
返信
6,920件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

program and data flash is protected by ECC too.

Are you aware of this application note?

https://www.nxp.com/docs/en/application-note/AN12522.pdf

It should answer all your questions.

Regards,

Lukas

 

0 件の賞賛
返信
6,905件の閲覧回数
andals
Contributor I

@lukaszadrapa 

After reading the application note, it is still a bit unclear to us about the single-bit fault for flash. Following information exist in the application note:

The ECC logic implemented in the S32K1xx Flash memory can correct single-bit fault automatically and can detect multiple-bit fault in each NVM sections. The multiple-bit fault is enabled using the FERCNFG[DFDIE] bit. When the multiple-bit error is detected, the FERSTAT[DFDIF] flag is set, and the interrupt request is generated.

  • Since the formulation above is "can correct single-bit fault automatically", is there any action needed to turn on the correction?
  • Is there any reporting of single-bit faults in flash?

Best regards,

André

 

0 件の賞賛
返信
6,897件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi André,

yes, single bit errors are automatically corrected. This feature can't be turned off.

Reporting can be enabled in Error Reporting Module in CR0 register if needed.

Regards,

Lukas

 

0 件の賞賛
返信
6,891件の閲覧回数
andals
Contributor I

Hi Lukas,

Then our doubts regarding enabling of single bit error correction are clear, thank you!

Regarding Error Reporting, the latest Reference Manual for S32K (Rev. 12.1, 02/2020) states that the mentioned register is used only for RAM error reporting. Is this not the case?

 

chip_specific.png

reg_cr0.png

Best regards,

André

0 件の賞賛
返信
6,872件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

That's a good point, you are right. Sorry, I mismatched that with another devices where it is possible.

I just confirmed that there's no flag for single bit error. Only double bit error can be reported on flash.

Regards,

Lukas

 

0 件の賞賛
返信
6,867件の閲覧回数
andals
Contributor I

Thank you Lukas for your fast support in this matter! 

Have a nice evening.

Best regards,

André

0 件の賞賛
返信
6,914件の閲覧回数
andals
Contributor I

@lukaszadrapa 

Thank you for the quick reply! We have not seen this specific application note, we will review it and hopefully it should clear out our doubts.

Best regards,

André

0 件の賞賛
返信