S32K EB tresos disable SPI production error
Hi,
I am using S32K EB tresos for SPI driver configuration,when configure the “SpiAutosarExt”, we can
disable SPI production error reporting,this is not compliant with autosar SPI specification.
Could you pls tell me why,and the purpose of “disable SPI DEM report error”.
Best regards,
Jack

Hello,
The SpiDisableDemErrorReportStatus is non-AUTOSAR feature, which NXP has implemented for customers who don't want DEM error report in their application by special purposes. If you are implementing a fully AUTOSAR compliant, then let the SpiDisableDemErrorReportStatus un-tick.

Hi @Simin
I think that this is very clear. It is just a AutosarExt. And the driver give user a feature to disable the DEM report error. Then user can choose enable or disable it.
Best regards,
Hung