freertos+s32k

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

freertos+s32k

Jump to solution
3,481 Views
kalajiao
Contributor II

I joined the freertos on s32k board, and then create a simple task in it as well as an interrupt the callback function, want to test the recovery of the suspension of tasks and inside the interrupt, but there was a problem, is at the time of task, stuck in a function out, don't know why, as the chart

QQ截图20210722140257.png

This is my overall callback function

中断回复任务出不来的地方.png

This is where the loop goes all the way up here

0 Kudos
Reply
1 Solution
3,475 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Please check the answer in: About the button
Please try to clear interrupt flag in callback(buttonisr).

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

Tags (1)
0 Kudos
Reply
1 Reply
3,476 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Please check the answer in: About the button
Please try to clear interrupt flag in callback(buttonisr).

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

Tags (1)
0 Kudos
Reply