S32DS version 2.2 Error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32DS version 2.2 Error

ソリューションへジャンプ
4,788件の閲覧回数
sungjun
Contributor II

hello? NXP
I wonder if there is an errata for S32DS arm 2.2 version.
The S32DS I am currently using is shown in the photo below.
If you look at ProcessorExpert's clockMan, you can set DIV for Run/VLPR/HSRUN Mode in Interface clocks.

However, when I generate the value set through the UI, it does not match the value displayed in the actual code.
Is this an errata? Or is it handled separately by the sdk driver?

thank you

 

sungjun_0-1706674419683.pngsungjun_0-1706674419683.png

sungjun_1-1706674455162.pngsungjun_1-1706674455162.pngsungjun_2-1706674518933.pngsungjun_2-1706674518933.png

 

 

0 件の賞賛
返信
1 解決策
4,750件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

Hi@sungjun

This picture comes from S32 Design Platform V3.4 & RTM 4.0.X.

you have to install the above IDE and SDK then you can see the picture in clock setting page.

 

元の投稿で解決策を見る

0 件の賞賛
返信
9 返答(返信)
4,782件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

Hi@sungjun

Only the files in this folder are configuration files generated by S32 DS

Senlent_0-1706679455411.pngSenlent_0-1706679455411.png

 

0 件の賞賛
返信
4,774件の閲覧回数
sungjun
Contributor II

I know. can you see above picture and compare SDK UI div value and c code.

0 件の賞賛
返信
4,771件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

Hi@sungjun

ok, could you please tell me the name of the file in the picture your provided and the SDK version you're using?

0 件の賞賛
返信
4,767件の閲覧回数
sungjun
Contributor II

File name : clockMan1.c

Sdk : 

S32 Design Studio for ARM

Version: 2.2
Build id: 200116

Copyright Freescale Semiconductor 2016. All rights reserved.
Copyright 2017-2020 NXP

Visit http://www.nxp.com/


This product includes software developed by the Eclipse Foundation http://www.eclipse.org/

This product includes software developed by the Apache Software Foundation http://apache.org/

 

The related information was written using the photo in the first question. Can't you see it?

0 件の賞賛
返信
4,762件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

Hi@sungjun

I see no problem here

Senlent_1-1706683065752.pngSenlent_1-1706683065752.png

 

0 件の賞賛
返信
4,758件の閲覧回数
sungjun
Contributor II

The question was why the Div numbers in the photos were different.

sungjun_0-1706683220110.pngsungjun_0-1706683220110.png

After checking again, it appears that the SDK UI is a DIV based on SPLL and clockMan1.c is a DIV based on the system clock.

It is also divided into SYS_CLK in RM's Blockdiagram.
Is that right?

 

sungjun_1-1706683651150.pngsungjun_1-1706683651150.png

 

 

0 件の賞賛
返信
4,756件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

Hi@sungjun

Senlent_0-1706684047176.pngSenlent_0-1706684047176.png

 

0 件の賞賛
返信
4,752件の閲覧回数
sungjun
Contributor II

Thanks to you, my problem was solved.
I would like to ask one more question.
I also want to check like the picture below, where is the data?

sungjun_0-1706684318049.pngsungjun_0-1706684318049.png

 

0 件の賞賛
返信
4,751件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

Hi@sungjun

This picture comes from S32 Design Platform V3.4 & RTM 4.0.X.

you have to install the above IDE and SDK then you can see the picture in clock setting page.

 

0 件の賞賛
返信