S32DS v3.4 Clock tool not working correctly?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32DS v3.4 Clock tool not working correctly?

1,368 Views
bananium
Contributor I

I try to configure the clocks with the clock tool in S32DS v3.4 and it says there are no errors, and everything should be in line with the S32K144 datasheet, yet I get STATUS_ERROR from CLOCK_DRV_Init function.

Is this a known issue or what might I be doing wrong? Is the tool producing invalid configurations?

And is there a way to get more information why the clock initialization fails?

0 Kudos
Reply
3 Replies

1,363 Views
bananium
Contributor I

I now have core clock configured as 15.6MHz yet through an SDK function the device reports 78MHz. The changes don't take effect.

0 Kudos
Reply

1,317 Views
_Leo_
NXP TechSupport
NXP TechSupport

Hi,

Thank you so much for your interest in our products and for using our community.

Regarding the clock issue, please share your project to test the issue and to see in more detail what you are doing.

Regarding S32K144 working on S32DS 3.6 please refer to the following community post:

https://community.nxp.com/t5/S32-Design-Studio/S32K1xx-SDK-in-S32DS/td-p/2032492

Have a nice day!

0 Kudos
Reply

1,365 Views
bananium
Contributor I

It's like sometimes it works and other times it doesn't. Sometimes changes have an affect, other times they don't. Seems like a defective tool.

And I can't install v3.6 because it is impossible to get it to work with S32K1.

0 Kudos
Reply