S32DS failed to compile after loading tcpip_stack

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32DS failed to compile after loading tcpip_stack

ソリューションへジャンプ
3,745件の閲覧回数
shunyizhang
Contributor IV

shunyizhang_0-1704974077539.pngshunyizhang_1-1704974103874.png

RTD:3.0.0

S32DS:V3.5

 

Hi,NXP

I am using the IDE's own tcpip_stack, after loading the components and configuring the relevant Settings, the compiler appeared the problem, trying to find the cause, and finally did not solve, want to ask NXP engineers, the problem is not because a setting is not paired, resulting in errors, please help to point out, thank you ~

 

 

 

0 件の賞賛
返信
1 解決策
3,563件の閲覧回数
shunyizhang
Contributor IV

shunyizhang_0-1705625176601.png

I've solved the problem. This place can't be zero.
Thank you so much for your support.

元の投稿で解決策を見る

0 件の賞賛
返信
9 返答(返信)
3,663件の閲覧回数
NamLee
NXP Employee
NXP Employee

Hi shunyizhang,

Sorry for this inconvenience.

Please help me try workaround this error by delete this warning flag

Namm_0-1705481565721.png

Please give me exact version of RTD and tcpip_stack version that you're using. About DS, which update site version of DS that you've installed?

I understand you're using RTD example or any project?

Please give me details for checking directly.

Thank you,

Nam.

 

0 件の賞賛
返信
3,661件の閲覧回数
shunyizhang
Contributor IV

shunyizhang_0-1705482798086.png

shunyizhang_1-1705482853278.png

The compiled project is my own creation, RTD, S32DS, tcpip_Stack version see the picture above.

 

 

0 件の賞賛
返信
3,656件の閲覧回数
NamLee
NXP Employee
NXP Employee
Thanks for your quick response.
I understand that you are developing for K314 with TCPIP_stack 1.0.3 HF01 (latest). Is it possible if you can share your project to me?
Thank you,
Nam.
0 件の賞賛
返信
3,653件の閲覧回数
shunyizhang
Contributor IV

shunyizhang_0-1705483568913.png

 

Yes, I am creating a tcpip project based on S32K314; Since the company's computer has encryption software, I can't share my project for you to review, but I can share the screenshot to you, see the picture above, I only added these components, after the configuration, the initial compilation alarm appeared, but I repeatedly consulted the contents of the components, and never found the configuration that can eliminate the alarm.

0 件の賞賛
返信
3,648件の閲覧回数
NamLee
NXP Employee
NXP Employee
Got it. So can you show me the declaration of function vTaskSetThreadLocalStoragePointer?
Is that one of driver's stub functions?
Thank you,
Nam.
0 件の賞賛
返信
3,635件の閲覧回数
shunyizhang
Contributor IV

shunyizhang_0-1705484755896.png

Is that it?

 

0 件の賞賛
返信
3,590件の閲覧回数
NamLee
NXP Employee
NXP Employee

Hi,

I checked with the lwip example and compile it, i added RTOS simply like you. The compiling done without errors.

Namm_0-1705566393523.png

Namm_3-1705566803247.png

 

I installed K3xx dev package, K3 3.0.0 P07, DS update site 3.5.2, service pack EAR2, then RTOS 10.5.1 and tcpip_stack 3.1.0

Namm_2-1705566699052.png

Namm_1-1705566579911.png

Did you tried with K344 one? Is that the same issue happened?

Thank you,

Nam.

 

0 件の賞賛
返信
3,587件の閲覧回数
NamLee
NXP Employee
NXP Employee

Also, please help me to try:

- Increase this param higher than 0.

Namm_0-1705567477159.png

 

- Remove Warning flag mentioned in compiler errors.

Thank you,

Nam.

0 件の賞賛
返信
3,564件の閲覧回数
shunyizhang
Contributor IV

shunyizhang_0-1705625176601.png

I've solved the problem. This place can't be zero.
Thank you so much for your support.

0 件の賞賛
返信