S32DS V3.4 cannot use PE Micro for debugging

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32DS V3.4 cannot use PE Micro for debugging

2,434件の閲覧回数
xqcnhz
Contributor I

hello,

I got an error when I used PE Micro to debug,I have installed these plugins:

1133.png1133.png

S32DS cannot use PE Micro for debugging, the error message is as follows:

1122.png

0 件の賞賛
返信
1 返信

2,422件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi xqcnhz,

Have you try to debug the demo projects in SDK?
I can debug hello_world_s32k144 with onboard OpenSDA and external PE Multilink without issue.
Would you please compare the debug configuration between your project and these demos?

Debug Configurations.pngDebug Configurations.png

Debug Configurations Debugger.pngDebug Configurations Debugger.png

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

0 件の賞賛
返信