S32DS Pin Configuration tool S32K358

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32DS Pin Configuration tool S32K358

Jump to solution
7,851 Views
Juanda
Contributor II

Hello,

I'm a PCB designer and I'm trying to make the Pins configuration tool work for the S32K358 MCU.

The IDE says that I need to select a MCU but there's no option for that. Do I need to install any other package?

 

Captura1.PNGCaptura2.PNG

 

I know there's an excel file with all the pins listed but I'm looking for something faster and interactive.

Thank you for your help!

Juan

Tags (2)
0 Kudos
Reply
1 Solution
7,619 Views
Juanda
Contributor II

Well, something like that seemed to be the problem. I cannot tell you which were the conflicting files because I removed all the extensions prior to your reply. Although I updated everithing using the update tool from the S32DS.

Solution was removing all extensions and updates and installing the SW package from the "RD-HVBMSCT800BUN reference design bundle" so probably I was missing something?

That did the trick for since I only need to see the pins with the configuration tool.

View solution in original post

0 Kudos
Reply
9 Replies
7,642 Views
Juanda
Contributor II

Admin rights did not work...

0 Kudos
Reply
7,636 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @Juanda 

Sorry for the inconvenience.

I am still not able to replicate your issue. 

This situation could be caused because the development package version. Please try to update to the most recent release. You can download it from S32K3 Standard Software -> Automotive SW - S32K3 - S32 Design Studio -> S32 Design Studio 3.5.0 Development Package with support for S32K3xx devices (released on March 31, 2023).

0 Kudos
Reply
7,620 Views
Juanda
Contributor II

Well, something like that seemed to be the problem. I cannot tell you which were the conflicting files because I removed all the extensions prior to your reply. Although I updated everithing using the update tool from the S32DS.

Solution was removing all extensions and updates and installing the SW package from the "RD-HVBMSCT800BUN reference design bundle" so probably I was missing something?

That did the trick for since I only need to see the pins with the configuration tool.

0 Kudos
Reply
7,823 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @Juanda 

From the images you share, the only step you are missing is selecting your project in Config Tools.

VaneB_0-1691186279626.png

If you are going to implement your project with MCAL, the pin configurations need to be made at the Peripherals tool. 

 

B.R.

VaneB

 

0 Kudos
Reply
7,793 Views
Juanda
Contributor II

Hello @VaneB,

For selecting the project i have these option but nothing happens when I click on them.

Captura3.png

Maybe I'm doing something wrong when creating the project?

Thank you in advance!

Juan

0 Kudos
Reply
7,785 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @Juanda 

Could you share an image of the view of pin tools when you select any of the projects?

Also, could you share how the project was created? I am not able to replicate your problem. 

 

0 Kudos
Reply
7,769 Views
Juanda
Contributor II

Hey @VaneB,

Nothing happens when I click on any of those projects.

Juanda_0-1691475256066.png

 

This is how I created the project:

Juanda_1-1691475392386.pngJuanda_2-1691475435542.pngJuanda_3-1691475516948.png

 

0 Kudos
Reply
7,759 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @Juanda 

I think you are still not selecting the project in Config Tools because the first shared image says <Select Project>. 

VaneB_0-1691526628835.png

VaneB_1-1691527172132.png

0 Kudos
Reply
7,724 Views
Juanda
Contributor II

I do click on the projects but nothing happens. It goes back to <Select Project>.

I'll try opening the program with admin rights and reinstalling the extensions.

0 Kudos
Reply