S32DS Change processor type

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32DS Change processor type

3,788 Views
koehlerl
Contributor IV

Hi,

In my project I changed the processor type from S32K144 to S32K146. It all worked until I can't change the SDK.

In the SDK path in the project tree is the right S32K146 MCU.

koehlerl_0-1681799930670.pngkoehlerl_0-1681799930670.png

I also have changed the defined symbols for preprocessor.

But I can't chnage the SDK in the Project settings:

koehlerl_1-1681800188133.pngkoehlerl_1-1681800188133.png

The symbol means:

SDK does not support processor or core required by the project. Cannot attach.  

What do I have to do to be able to change the SDK in the project settimgs?

BR

Lutz

0 Kudos
Reply
5 Replies

3,752 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@koehlerl

I reproduced it, it is indeed like this, this really cannot be changed
But this does not affect the compilation of the project, I think this is not a bug,

0 Kudos
Reply

3,781 Views
Senlent
NXP TechSupport
NXP TechSupport
0 Kudos
Reply

3,773 Views
koehlerl
Contributor IV

I have done all the steps from post

https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-Change-the-CPU-Derivative-in-an-... 

and the project works but the sdk project setting is not right respectively I cannot attach to S32K146.

BR Lutz 

0 Kudos
Reply

3,768 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@koehlerl

Can you take a screenshot?
In fact, this operation is not very convenient, and some files need to be deleted and added. I suggest to create a new S32K146 project directly, and refer to the configuration of the old project. This work is very simple and there will be no accidental errors.

0 Kudos
Reply

3,766 Views
koehlerl
Contributor IV

The sreenshot

koehlerl_0-1681810843276.pngkoehlerl_0-1681810843276.png

I cannot attach the S32K146

0 Kudos
Reply