S32DS Activation Code Error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32DS Activation Code Error

2,092 Views
seungmin
Contributor I

I was using S32 Design Studio for S32 Platform 3.4 well until a week ago.
An error related to the license occurred, and when I entered the Activation Code, I received the following error message.

'S32 Desgin Studio for S32 platform 3.4 License missing'

Attached the .metadata file.

seungmin_0-1730858047708.png

 

0 Kudos
Reply
4 Replies

2,061 Views
seungmin
Contributor I

Nothing has been installed except for recent Windows updates.
S32ds is allowed in the firewall.
To create the offline request file, I clicked the check box and pressed activate, and it comes out as shown in the picture below. Is this the wrong way?

seungmin_0-1730882079363.png

 

0 Kudos
Reply

1,967 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

please try to delete content of c:\ProgramData\FLEXnet\ folder. The folder is hidden by default. 

0 Kudos
Reply

2,065 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

You can try offline activation.

Did you change anything on your PC? Some firewall, server settings or some sw which can prevent connection to server?

https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-Activate-S32-Design-Studio/ta-p/...

Best regards,

Peter

0 Kudos
Reply

2,022 Views
seungmin
Contributor I
I attached an answer to your proposal.
Please check the answer.
0 Kudos
Reply