S32DS Activation Code Error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32DS Activation Code Error

1,991件の閲覧回数
seungmin
Contributor I

I was using S32 Design Studio for S32 Platform 3.4 well until a week ago.
An error related to the license occurred, and when I entered the Activation Code, I received the following error message.

'S32 Desgin Studio for S32 platform 3.4 License missing'

Attached the .metadata file.

seungmin_0-1730858047708.pngseungmin_0-1730858047708.png

 

0 件の賞賛
返信
4 返答(返信)

1,960件の閲覧回数
seungmin
Contributor I

Nothing has been installed except for recent Windows updates.
S32ds is allowed in the firewall.
To create the offline request file, I clicked the check box and pressed activate, and it comes out as shown in the picture below. Is this the wrong way?

seungmin_0-1730882079363.pngseungmin_0-1730882079363.png

 

0 件の賞賛
返信

1,866件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

please try to delete content of c:\ProgramData\FLEXnet\ folder. The folder is hidden by default. 

0 件の賞賛
返信

1,964件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

You can try offline activation.

Did you change anything on your PC? Some firewall, server settings or some sw which can prevent connection to server?

https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-Activate-S32-Design-Studio/ta-p/...

Best regards,

Peter

0 件の賞賛
返信

1,921件の閲覧回数
seungmin
Contributor I
I attached an answer to your proposal.
Please check the answer.
0 件の賞賛
返信