[S32DS 3.6.1] Example Code disappear !?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[S32DS 3.6.1] Example Code disappear !?

1,340 Views
CY9
Contributor IV

餓死抬頭 

As the title 

 

I'd install brand new S32DS v3.6.1 on brand new OS.

I CAN *NOT* find any example project out : 

What's wrong !?? 

 

CY9_0-1787706296255.png

 

S32DS-S32PLATFORM S32DS-ARM  

0 Kudos
Reply
14 Replies

1,338 Views
CY9
Contributor IV

After install `S32SDK_S32K1xx_RTM_4.0.2.exe` , 

The situation remains the same. 

0 Kudos
Reply

1,319 Views
Robin_Shen
NXP TechSupport
NXP TechSupport
Hi
If you must use S32K1 SDK RTM 4.0.3, then please install S32K1 SDK RTM 4.0.3 in S32DS v3.4 by refer to the discussion in Where can I find it?S32_SDK_S32K1xx_RTM_4.0.3 .

S32DS v3.4 can be download by click S32 Design Studio – Windows/Linux -> S32 Design Studio IDE -> Previous -> S32 Design Studio for S32 Platform v.3.4 -> S32DS.3.4_b201217_win32.x86_64.exe
 
It is not recommended to install S32K1 SDK 4.0.x in S32DS v3.5 or v3.6. According to the currently available information, we don’t have any plan to integrate S32SDK S32K1XX 4.0.x into S32DS 3.5 or above version.
 
For new project development,  I recommend you to use the latest S32K1 RTD in S32DS v3.6.10. The old SDK will not be updated to fix bugs.
Please download Real-Time Drivers for S32K1 -> Automotive SW - S32K1_S32M24x - Real-Time Drivers for Cortex-M -> S32K1_S32M24X Real Time Drivers AUTOSAR R21-11 Version 3.0.0 ->  SW32K1_S32M24x_RTD_R21-11_3.0.0_D2503_DesignStudio_updatesite.zip
 
Please refer to the instructions in the video(How To Download, Install and Configure the RTD 5.0.0 with S32 Design Studio 3.6.0) to install the specific version of S32K1 RTD that you need. 
 
And don't forget to install NXP GCC for Arm Embedded Processors v10.2 build 1728
NXP GCC for Arm Embedded Processors v10.2 build 1728.png
Best Regards,
Robin
0 Kudos
Reply

1,288 Views
anbn
Contributor II

NXP, please confirm. Is the S32K1 SDK deprecated?

Tags (1)
0 Kudos
Reply

1,286 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

It has been replaced by the S32K1 RTD since the last version, S32K1 SDK 4.0.3.

0 Kudos
Reply

1,282 Views
anbn
Contributor II

But that doesn't include example code, correct?

0 Kudos
Reply

1,278 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

No. If the S32K1 RTD is installed correctly, the examples will be displayed in S32DS v3.6.x.

Here are the examples of S32K1 RTD:

S32K1 RTD 3.0.0.png

1,268 Views
anbn
Contributor II

Is it Windows-only? RTDs don't show up when adding the updatesite in Linux. 

Tags (1)
0 Kudos
Reply

1,309 Views
CY9
Contributor IV

Your S32DS report version to OS is 3.6.1 !! not `10` too...

 

CY9_0-1787722320774.png

 

CY9_1-1787722371649.png

 

0 Kudos
Reply

1,307 Views
CY9
Contributor IV

I am trying to abandom uninstall this SHxT version ... 

 

Will NEVER using this version . 

 

Thanks for your comments. 

0 Kudos
Reply

1,312 Views
CY9
Contributor IV

I am using S32DS 3.6.10 ...

I don't know why it's default install path = `C:\NXP\S32DS.3.6.1\` , not `C:...6.10\` 

 

My problem is : 

the "Example Project" disappear !! 

even already install S32K1_S32M24X Real Time Drivers in this instruction: https://community.nxp.com/t5/S32-SDK/S32K1XX-SD...

 

0 Kudos
Reply

1,310 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

1. You will not see the S32K1 SDK 4.0.x in S32DS v3.6.x under any circumstances. Installing S32SDK_S32K1xx_RTM_4.0.2.exe will not make the SDK example appear in S32DSv3.6.x. If you need the S32K1 SDK, please install it according to my previous answer.

2. If the S32K1 RTD is not installed correctly, the example will also not be visible in S32DS v3.6.x. Please install SW32K1_S32M24x_RTD_R21-11_3.0.0_D2503_DesignStudio_updatesite.zip according to the method shown in the video I provided earlier.

0 Kudos
Reply

1,300 Views
CY9
Contributor IV

Because it cause another problem : 

 

My previous project is create by RTM 4.0.2 , 

I can NOT open previous project , even using import function. 

 

The best fastest solotion for me is install previous version + RTM 4.0.2 . 

This SHxT waste me too much time on it. 

 

CY9_2-1787708167310.png

0 Kudos
Reply

1,297 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Then please download S32DSv3.4 and then install SW32K1_S32DS_3.4.1_D2106.zip. This software package can be downloaded from the download page for S32DS.3.4_b201217_win32.x86_64.exe.

S32DS v3.4 SW32K1_S32DS_3.4.1_D2106 S32K1 SDK 4.0.2.png

The SW32K1_S32DS_3.4.1_D2106.zip file contains the S32 SDK for S32K1xx RTM 4.0.2. For installation instructions, please refer to: S32 Design Studio v3.4 S32K1 Service Pack 1 released!

0 Kudos
Reply

1,331 Views
CY9
Contributor IV

???

 

CY9_0-1787707907582.png

 

No RTM !? even already installed !?

Install RTM FAIL !?? 

CY9_1-1787708009334.png

 

cause : 

CY9_2-1787708167310.png

 

``` 

# grep -in "RTM" * .* 

PrjXX_LinMaster_144.mex:6: <mcu_data>s32sdk_s32k1xx_rtm_402</mcu_data>
.cproject:7: <stringMacro name="S32_SDK_PATH" type="VALUE_TEXT" value="${eclipse_home}../S32DS/software/S32SDK_S32K1XX_RTM_4.0.2"/>
.cproject:201: <stringMacro name="S32_SDK_PATH" type="VALUE_TEXT" value="${eclipse_home}../S32DS/software/S32SDK_S32K1XX_RTM_4.0.2"/>
.project:321: <locationURI>S32SDK_S32K1XX_RTM_4.0.2/middleware/lin/doxygen/LIN_Stack_Architecture.png</locationURI>
.project:326: <locationURI>S32SDK_S32K1XX_RTM_4.0.2/middleware/lin/doxygen/LIN_Stack_Configuration_Data.png</locationURI>
.project:331: <locationURI>S32SDK_S32K1XX_RTM_4.0.2/middleware/lin/doxygen/lin_stack.dox</locationURI>
.project:336: <locationURI>S32SDK_S32K1XX_RTM_4.0.2/rtos/osif/doxygen/osif.dox</locationURI>
.project:376: <locationURI>S32SDK_S32K1XX_RTM_4.0.2/platform/drivers/src/clock/doxygen/clock_manager.dox</locationURI>
.project:381: <locationURI>S32SDK_S32K1XX_RTM_4.0.2/platform/drivers/src/edma/doxygen/edma_driver.dox</locationURI>
.project:386: <locationURI>S32SDK_S32K1XX_RTM_4.0.2/platform/drivers/src/interrupt/doxygen/interrupt.dox</locationURI>
.project:391: <locationURI>S32SDK_S32K1XX_RTM_4.0.2/platform/drivers/src/lin/doxygen/lin.dox</locationURI>
.project:396: <locationURI>S32SDK_S32K1XX_RTM_4.0.2/platform/drivers/src/lptmr/doxygen/lptmr.dox</locationURI>
.project:401: <locationURI>S32SDK_S32K1XX_RTM_4.0.2/platform/drivers/src/lptmr/doxygen/lptmr_driver.dox</locationURI>
.project:406: <locationURI>S32SDK_S32K1XX_RTM_4.0.2/platform/drivers/src/pins/doxygen/pins.dox</locationURI>
.project:411: <locationURI>S32SDK_S32K1XX_RTM_4.0.2/platform/drivers/src/clock/S32K1xx/doxygen/clock_S32K1xx.dox</locationURI>
.project:417: <value>file:/${eclipse_home}../S32DS/software/S32SDK_S32K1XX_RTM_4.0.2</value>

``` 

0 Kudos
Reply