S32146 CAN FD issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32146 CAN FD issue

4,086 Views
chandan_uv
Contributor III

Hello, I want to CAN0 of S32146 in CAN-FD mode. Initially I am using CAN0 as CAN 2.0 and working fine. But when I am using code in S32146, getting stuff error. I just modified the .fd enable, . payload and .data_length. Below is the code

 

2.png1.png

 

 

status_t host_can_init(void)
{
    status_t ret = STATUS_SUCCESS;
	
		
		flexcan_user_config_t can_500kbps_init_cfg = 
    {
        .fd_enable =true,
        .pe_clock = FLEXCAN_CLK_SOURCE_PERIPH,
        .max_num_mb = 4, //8,
        .num_id_filters = FLEXCAN_RX_FIFO_ID_FILTERS_8,
        .is_rx_fifo_needed = false,
        .flexcanMode = FLEXCAN_NORMAL_MODE,
        .payload = FLEXCAN_PAYLOAD_SIZE_64 , //FLEXCAN_PAYLOAD_SIZE_8,
        .bitrate = {
            .propSeg    = 3U,
            .phaseSeg1  = 10U,
            .phaseSeg2  = 7U,
            .preDivider = 9U,
            .rJumpwidth = 1U
        },
        .bitrate_cbt = {
            .propSeg    = 3U,
            .phaseSeg1  = 10U,
            .phaseSeg2  = 7U,
            .preDivider = 9U,
            .rJumpwidth = 1U
        },
		
				
				/*
			        .bitrate = {
            .propSeg    = 3U,
            .phaseSeg1  = 1U,
            .phaseSeg2  = 2U,
            .preDivider = 3U,
            .rJumpwidth = 1U
        },
        .bitrate_cbt = {
            .propSeg    = 3U,
            .phaseSeg1  = 1U,
            .phaseSeg2  = 2U,
            .preDivider = 3U,
            .rJumpwidth = 1U
        },
				*/

        .transfer_type = FLEXCAN_RXFIFO_USING_INTERRUPTS,
        .rxFifoDMAChannel = 0, 
    };
	
		FLEXCAN_DRV_Deinit(HOST_CAN_INST);
    /* CAN interface initialization */
    ret = FLEXCAN_DRV_Init(HOST_CAN_INST, &host_can_state, &can_500kbps_init_cfg);
    return ret;
}


void can_if_init_host (void)
{
    flexcan_data_info_t data_info =
    {
       .data_length = 64U,
       .msg_id_type = FLEXCAN_MSG_ID_STD,
       .fd_enable   = true,
       .enable_brs  = false,
       .fd_padding  = 0U
    };
    
   DEV_ASSERT(FLEXCAN_DRV_ConfigRxMb(HOST_CAN_INST, HOST_RX_MBX, &data_info, RX_HOST_MSG_ID) == STATUS_SUCCESS );
   FLEXCAN_DRV_SetRxMbGlobalMask(HOST_CAN_INST, FLEXCAN_MSG_ID_STD, RX_HOST_MSG_ID);
   DEV_ASSERT(FLEXCAN_DRV_SetRxIndividualMask(HOST_CAN_INST, FLEXCAN_MSG_ID_STD, HOST_RX_MBX, RX_HOST_MSG_ID) == STATUS_SUCCESS );
}

status_t can_send(uint8_t instance, uint8_t mb_idx, uint8_t *tx_data, uint32_t len, uint32_t msg_id, flexcan_msgbuff_id_type_t id_type)
{
	status_t send_status = STATUS_SUCCESS; 
	//bool sucess = false;
    
	flexcan_data_info_t txdata_info =
	{
		.data_length = len,
		.msg_id_type = id_type,
		.enable_brs  = false,
		.fd_enable   = false,
		.fd_padding  = 0U,
		.is_remote = false
	};
	
	if(instance == HOST_CAN_INST){
		txdata_info.fd_enable   = true;
	}
	
	if( FLEXCAN_DRV_GetTransferStatus(instance, mb_idx) != STATUS_BUSY ){
	/* Configure TX message buffer with index TX_MBX and msg_id*/
    FLEXCAN_DRV_ConfigTxMb(instance, mb_idx, &txdata_info, msg_id);
	/* Start transimitting data */	
	send_status = FLEXCAN_DRV_Send(instance, mb_idx, &txdata_info, msg_id, tx_data);
	
	}
	return send_status;
}

 

0 Kudos
Reply
7 Replies

4,072 Views
chandan_uv
Contributor III

Updated CAN bit rate configuration as below, still similar issue 

 

.bitrate = {
.propSeg = 4U,
.phaseSeg1 = 7U,
.phaseSeg2 = 1U,
.preDivider = 9U,
.rJumpwidth = 1U
},
.bitrate_cbt = {
.propSeg = 4U,
.phaseSeg1 = 7U,
.phaseSeg2 = 1U,
.preDivider = 9U,
.rJumpwidth = 1U
},

0 Kudos
Reply

4,062 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@chandan_uv

If possible, please provide the entire project and I will test it for you.

0 Kudos
Reply

4,059 Views
chandan_uv
Contributor III
Its not possible for me to share as shared code is a part of project.
0 Kudos
Reply

4,056 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@chandan_uv

the bitrate configuration is not right from your description.

have a try below setting

Senlent_0-1698142204118.png

and i didn't find any more issues in the picture you provided.

if still have issues,please provided the demo code,

0 Kudos
Reply

4,052 Views
chandan_uv
Contributor III
HI @Senlent, Clock is 80MHZ for me and below are the bit rate configuration

.bitrate = {
.propSeg = 4U,
.phaseSeg1 = 7U,
.phaseSeg2 = 1U,
.preDivider = 9U,
.rJumpwidth = 1U
},
.bitrate_cbt = {
.propSeg = 4U,
.phaseSeg1 = 7U,
.phaseSeg2 = 1U,
.preDivider = 9U,
.rJumpwidth = 1U
},
0 Kudos
Reply

4,036 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@chandan_uv

please have a try below settings.

Senlent_0-1698197183378.png

 

0 Kudos
Reply

3,791 Views
chandan_uv
Contributor III

@Senlent I tried but still same issue.

 

 

status_t host_can_init(void)
{
    status_t ret = STATUS_SUCCESS;

	/* Configuration for 500kbps CAN bit rate */
	flexcan_user_config_t can_500kbps_init_cfg = 
    {
        .fd_enable =true,
        .pe_clock = FLEXCAN_CLK_SOURCE_PERIPH,
        .max_num_mb = 4, //8,
        .num_id_filters = FLEXCAN_RX_FIFO_ID_FILTERS_8,
        .is_rx_fifo_needed = false,
        .flexcanMode = FLEXCAN_NORMAL_MODE,
        .payload = FLEXCAN_PAYLOAD_SIZE_64 , //FLEXCAN_PAYLOAD_SIZE_8,
				.bitrate = {
            .propSeg    = 7U,
            .phaseSeg1  = 4U,
            .phaseSeg2  = 1U,
            .preDivider = 9U,
            .rJumpwidth = 1U
        },
        .bitrate_cbt = {
            .propSeg    = 7U,
            .phaseSeg1  = 4U,
            .phaseSeg2  = 1U,
            .preDivider = 9U,
            .rJumpwidth = 1U
        },
			

        .transfer_type = FLEXCAN_RXFIFO_USING_INTERRUPTS,
        .rxFifoDMAChannel = 0, 
    };
	
    /* CAN interface initialization */
    ret = FLEXCAN_DRV_Init(HOST_CAN_INST, &host_can_state, &can_500kbps_init_cfg);
		DEV_ASSERT(ret == STATUS_SUCCESS);
    return ret;
}


void can_if_init_host (void)
{
    flexcan_data_info_t data_info =
    {
       .data_length = 64U,
       .msg_id_type = FLEXCAN_MSG_ID_STD,
       .fd_enable   = true,
       .enable_brs  = false,
       .fd_padding  = 0U
    };
    
   DEV_ASSERT(FLEXCAN_DRV_ConfigRxMb(HOST_CAN_INST, HOST_RX_MBX, &data_info, RX_HOST_MSG_ID) == STATUS_SUCCESS );
   FLEXCAN_DRV_SetRxMbGlobalMask(HOST_CAN_INST, FLEXCAN_MSG_ID_STD, RX_HOST_MSG_ID);
   DEV_ASSERT(FLEXCAN_DRV_SetRxIndividualMask(HOST_CAN_INST, FLEXCAN_MSG_ID_STD, HOST_RX_MBX, RX_HOST_MSG_ID) == STATUS_SUCCESS );
		
}

 

 

I checked with custom python script to receive the data, able to get data but it is in the multiple of 4, like if I send 13, receiving 16 bytes.

chandan_uv_0-1701781750516.png

 

 

 

 

0 Kudos
Reply