MCU_HSE_SWT_RST_RESET

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCU_HSE_SWT_RST_RESET

1,140 Views
myehiash
Contributor I

S32K388 Eval Board resets with reason MCU_HSE_SWT_RST_RESET
- The Eval board resets only one time after the startup and then work normally
- Why this happens?
- I tried to write directly to DCMRWP1 register to disable the functional reset but nothing happened.
Update:
Also, Siul2_Port_Ip_Example_S32K388 which is supported from s32k388 package does the same behavior.
- The Software should toggle the LED on PTA0 10 times
- After powering up the LED starts with 3 blinks the resets and begin to blink 10 times

Tags (2)
0 Kudos
Reply
0 Replies