S32 design studio 3.6.4 compilation error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32 design studio 3.6.4 compilation error

Jump to solution
1,905 Views
aaz1234
Contributor II

Hello,

I am using S32 Design Studio 3.6.4 and attempting to flash the DIO example onto my RD-BESS1500BUN board for practice. The MCU on the board is S32K358, and I am using a J-Link debugger.

I installed the RTD S32K3xx drivers and integrated them into S32 Design Studio. After that, I imported the DIO example project provided with the RTD package. I opened the project’s .mex file in ConfigTools and generated/updated the code from there. 
But i kept on getting these errors

 

Capture.PNG

Tags (1)
0 Kudos
Reply
1 Solution
1,806 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@aaz1234

This isn't a complicated issue.

I've already helped you resolve the compilation problems.

You should check yourself to ensure that the hardware you're using and the PIN used in the demo are compatible with your hardware.

View solution in original post

0 Kudos
Reply
7 Replies
1,853 Views
aaz1234
Contributor II

I did that and now I just deleted the example and reloaded it. 

08:12:33 **** Incremental Build of configuration Debug_FLASH for project Dio_Example_S32K358 ****

make -j1 all

Building file: ../board/Tspc_Port_Ip_Cfg.c

Invoking: Standard S32DS C Compiler

arm-none-eabi-gcc "@board/Siul2_Port_Ip_Cfg.args" -MMD -MP -MF"board/Tspc_Port_Ip_Cfg.d" -MT"board/Tspc_Port_Ip_Cfg.o" -o "board/Tspc_Port_Ip_Cfg.o" "../board/Tspc_Port_Ip_Cfg.c"

Finished building: ../board/Tspc_Port_Ip_Cfg.c

 

Building file: ../RTD/src/Clock_Ip.c

Invoking: Standard S32DS C Compiler

arm-none-eabi-gcc "@RTD/src/Clock_Ip.args" -MMD -MP -MF"RTD/src/Clock_Ip.d" -MT"RTD/src/Clock_Ip.o" -o "RTD/src/Clock_Ip.o" "../RTD/src/Clock_Ip.c"

Finished building: ../RTD/src/Clock_Ip.c

 

Building file: ../RTD/src/Clock_Ip_Data.c

Invoking: Standard S32DS C Compiler

arm-none-eabi-gcc "@RTD/src/Clock_Ip.args" -MMD -MP -MF"RTD/src/Clock_Ip_Data.d" -MT"RTD/src/Clock_Ip_Data.o" -o "RTD/src/Clock_Ip_Data.o" "../RTD/src/Clock_Ip_Data.c"

Finished building: ../RTD/src/Clock_Ip_Data.c

 

Building file: ../RTD/src/Clock_Ip_Divider.c

Invoking: Standard S32DS C Compiler

arm-none-eabi-gcc "@RTD/src/Clock_Ip.args" -MMD -MP -MF"RTD/src/Clock_Ip_Divider.d" -MT"RTD/src/Clock_Ip_Divider.o" -o "RTD/src/Clock_Ip_Divider.o" "../RTD/src/Clock_Ip_Divider.c"

Finished building: ../RTD/src/Clock_Ip_Divider.c

 

Building file: ../RTD/src/Clock_Ip_DividerTrigger.c

Invoking: Standard S32DS C Compiler

arm-none-eabi-gcc "@RTD/src/Clock_Ip.args" -MMD -MP -MF"RTD/src/Clock_Ip_DividerTrigger.d" -MT"RTD/src/Clock_Ip_DividerTrigger.o" -o "RTD/src/Clock_Ip_DividerTrigger.o" "../RTD/src/Clock_Ip_DividerTrigger.c"

Finished building: ../RTD/src/Clock_Ip_DividerTrigger.c

 

Building file: ../RTD/src/Clock_Ip_ExtOsc.c

Invoking: Standard S32DS C Compiler

arm-none-eabi-gcc "@RTD/src/Clock_Ip.args" -MMD -MP -MF"RTD/src/Clock_Ip_ExtOsc.d" -MT"RTD/src/Clock_Ip_ExtOsc.o" -o "RTD/src/Clock_Ip_ExtOsc.o" "../RTD/src/Clock_Ip_ExtOsc.c"

Finished building: ../RTD/src/Clock_Ip_ExtOsc.c

 

Building file: ../RTD/src/Clock_Ip_FracDiv.c

Invoking: Standard S32DS C Compiler

arm-none-eabi-gcc "@RTD/src/Clock_Ip.args" -MMD -MP -MF"RTD/src/Clock_Ip_FracDiv.d" -MT"RTD/src/Clock_Ip_FracDiv.o" -o "RTD/src/Clock_Ip_FracDiv.o" "../RTD/src/Clock_Ip_FracDiv.c"

Finished building: ../RTD/src/Clock_Ip_FracDiv.c

 

Building file: ../RTD/src/Clock_Ip_Frequency.c

Invoking: Standard S32DS C Compiler

arm-none-eabi-gcc "@RTD/src/Clock_Ip.args" -MMD -MP -MF"RTD/src/Clock_Ip_Frequency.d" -MT"RTD/src/Clock_Ip_Frequency.o" -o "RTD/src/Clock_Ip_Frequency.o" "../RTD/src/Clock_Ip_Frequency.c"

Finished building: ../RTD/src/Clock_Ip_Frequency.c

 

Building file: ../RTD/src/Clock_Ip_Gate.c

Invoking: Standard S32DS C Compiler

arm-none-eabi-gcc "@RTD/src/Clock_Ip.args" -MMD -MP -MF"RTD/src/Clock_Ip_Gate.d" -MT"RTD/src/Clock_Ip_Gate.o" -o "RTD/src/Clock_Ip_Gate.o" "../RTD/src/Clock_Ip_Gate.c"

Finished building: ../RTD/src/Clock_Ip_Gate.c

 

Building file: ../RTD/src/Clock_Ip_IntOsc.c

Invoking: Standard S32DS C Compiler

arm-none-eabi-gcc "@RTD/src/Clock_Ip.args" -MMD -MP -MF"RTD/src/Clock_Ip_IntOsc.d" -MT"RTD/src/Clock_Ip_IntOsc.o" -o "RTD/src/Clock_Ip_IntOsc.o" "../RTD/src/Clock_Ip_IntOsc.c"

Finished building: ../RTD/src/Clock_Ip_IntOsc.c

 

Building file: ../RTD/src/Clock_Ip_Irq.c

0 [main] make (5492) child_copy: cygheap read copy failed, 0x0..0x80002A480, done 0, windows pid 5492, Win32 error 299

0 [main] make 1067 dofork: child -1 - forked process 5492 died unexpectedly, retry 0, exit code 0xC0000142, errno 11

make: *** [RTD/src/subdir.mk:157: RTD/src/Clock_Ip_Irq.o] Error 127

"make -j1 all" terminated with exit code 2. Build might be incomplete.

 

08:12:39 Build Failed. 1 errors, 0 warnings. (took 6s.336ms)

 

 
 

Screenshot 2026-03-24 081519.png

 

 

0 Kudos
Reply
1,844 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@aaz1234

0 [main] make 1067 dofork: child -1 - forked process 5492 died unexpectedly, retry 0, exit code 0xC0000142, errno 11

Based on this information, it seems to be a problem with your computer, most commonly caused by antivirus/security software interfering with a fork on Windows.

 

0 Kudos
Reply
1,834 Views
aaz1234
Contributor II

Hi,
I have tried with my personal laptop, its now building without errors and i have debugged it as well. but the LED is still not blinking... I used this setting

Debug config..png

0 Kudos
Reply
1,807 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@aaz1234

This isn't a complicated issue.

I've already helped you resolve the compilation problems.

You should check yourself to ensure that the hardware you're using and the PIN used in the demo are compatible with your hardware.

0 Kudos
Reply
1,857 Views
aaz1234
Contributor II

I’m using RTD 3.0.0 (AUTOSAR 4.7.0) on S32DS 3.6.4 This is the version i am using

And thats the error.

14:00:56 **** Incremental Build of configuration Debug_FLASH for project Dio_Example_S32K358 ****

make -j1 all

Building file: ../Project_Settings/Startup_Code/system.c

Invoking: Standard S32DS C Compiler

arm-none-eabi-gcc "@Project_Settings/Startup_Code/exceptions.args" -MMD -MP -MF"Project_Settings/Startup_Code/system.d" -MT"Project_Settings/Startup_Code/system.o" -o "Project_Settings/Startup_Code/system.o" "../Project_Settings/Startup_Code/system.c"

../Project_Settings/Startup_Code/system.c:46:10: fatal error: Platform_Types.h: No such file or directory

46 | #include "Platform_Types.h"

| ^~~~~~~~~~~~~~~~~~

compilation terminated.

make: *** [Project_Settings/Startup_Code/subdir.mk:42: Project_Settings/Startup_Code/system.o] Error 1

"make -j1 all" terminated with exit code 2. Build might be incomplete.

 

14:01:02 Build Failed. 2 errors, 0 warnings. (took 6s.216ms)

 

 

I was having another error during building the project and it was related to parallel build so i disable parallel build and chose these conf. but now it is gone

 

Screenshot 2026-03-24 075143.png

 

0 Kudos
Reply
1,855 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@aaz1234

"fatal error: Platform_Types.h: No such file or directory"

The error message indicates a missing file. Are you sure you clicked the "Update Code" to generate the configuration file?

0 Kudos
Reply
1,864 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@aaz1234

please tell me the RTD version you're using and could you please provide the error message in the screenshot.

0 Kudos
Reply