S32 Design Studio contiguous srec file

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32 Design Studio contiguous srec file

ソリューションへジャンプ
2,751件の閲覧回数
adria
Contributor I

Hello,

For S32K116, from the end of the interrupt vector table section until the start of the flash config section, there is a gap of memory unused. This gap is specified with zeros if a raw binary is generated. Instead, if srec file is generated, that space is not specified.

Is it possible to generate the srec file so it specifies all addresses so the whole addresses in the file are contiguous to each other?

Best regards,

Adria

0 件の賞賛
返信
1 解決策
2,701件の閲覧回数
dianabatrlova
NXP TechSupport
NXP TechSupport

Hello Adria,

 

You can use the srec_cat tool for this purpose, see section "FILLING THE BLANKS" in the last link.

Please refer to the links below:

I hope it helps.

Best Regards,

Diana

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,702件の閲覧回数
dianabatrlova
NXP TechSupport
NXP TechSupport

Hello Adria,

 

You can use the srec_cat tool for this purpose, see section "FILLING THE BLANKS" in the last link.

Please refer to the links below:

I hope it helps.

Best Regards,

Diana

0 件の賞賛
返信