S32 Design Studio 3.4 missing example projects

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32 Design Studio 3.4 missing example projects

2,584 Views
raneemrady
Contributor II

Hello, 

I recently downloaded the S32 Design studio 3.4 but I couldn't find any example projects:

raneemrady_0-1677018766836.png

 

Is there a problem with my installation or does this version come without example projects ?

0 Kudos
Reply
3 Replies

2,572 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi raneemrady,

Seems that you are using S32K1x, please install the latest S32 SDK for S32K1xx RTM 4.0.3 in S32DS 3.4 using Extensions and Updates  by refer to the discussion in How to connect SDK Version 4.0.3 to S32DS


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

2,564 Views
raneemrady
Contributor II

Okay so I can find the following in extensions and updates and I need to make sure I am installing the appropriate one:

1 - S32K1 RTD AUTOSAR 4.4 Version 1.0.1

2 - S32SDK S32K1XX RTM 4.0.3

Do they both contain example projects but one is autosar based and the other isn't ?

Or does only the S32SDK S32K1XX RTM 4.0.3 contain example projects ?

I

Tags (1)
0 Kudos
Reply

2,554 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Both contain example projects. The newer RTD combines SDK and MCAL environments in one software product.

0 Kudos
Reply