S32 Design Studio 3.4 error while installing extensions

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32 Design Studio 3.4 error while installing extensions

Jump to solution
2,345 Views
Prasanna2
Contributor I

Getting below error while installing extensions on S32 DS 3.4 for CANHUBK344 kit 

• S32K3 RTD AUTOSAR 4.4 Version 2.0.0
• S32K3xx development package Version 3.4.3

S32DS 3.4 Error First time.png

0 Kudos
Reply
1 Solution
2,244 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Do you see 3.4.3_D2112 S32 Design Studio for S32 Platform v.3.4 Update 3 with support for S32K3 devices(SW32K3_S32DS_3.4.3_D2112.zip) or 3.4.3_D2205 S32 Design Studio for S32 Platform v.3.4 Service Pack 4 with support for S32K341 device(SW32K3_S32DS_3.4.3_D2205.zip) after clicking Previous?

Previous SW32K3_S32DS_3.4.3_D2205 SW32K3_S32DS_3.4.3_D2112.png

View solution in original post

0 Kudos
Reply
5 Replies
2,202 Views
Prasanna2
Contributor I

Thanks i was able to do offline install of all the 3 extensions from the download link following the offline installation procedure as in the below link. Offline installation is more controlled procedure.

S32DS Extensions & Updates: Explanation and How To Use - NXP Community 

0 Kudos
Reply
2,292 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Please offline install S32K3 RTD 2.0.0 by refer to the discussion in S32K3 Unified Bootloader Build Issue


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply
2,280 Views
Prasanna2
Contributor I
Hello .. In the download page .. I find only this package
Development IDEs and Build Tools
S32 Design Studio 3.4 S32K1xx Service Pack 1
Rev 3.4.1_D2106
Jun 24, 2021
1 KB
SW32K1_S32DS_3.4.1_D2106
While in the link you shared above it is showing SW32K3_S32DS_3.4.3_D2112.zip

The download page i am searching for this offline package is here ..

https://www.nxp.com/design/design-center/software/automotive-software-and-tools/s32-design-studio-id....
0 Kudos
Reply
2,269 Views
Prasanna2
Contributor I
In the product download page i see 3.5.13 as the most recent offline package ..

https://nxp.flexnetoperations.com/control/frse/download?agree=Accept&element=6311641
0 Kudos
Reply
2,244 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Do you see 3.4.3_D2112 S32 Design Studio for S32 Platform v.3.4 Update 3 with support for S32K3 devices(SW32K3_S32DS_3.4.3_D2112.zip) or 3.4.3_D2205 S32 Design Studio for S32 Platform v.3.4 Service Pack 4 with support for S32K341 device(SW32K3_S32DS_3.4.3_D2205.zip) after clicking Previous?

Previous SW32K3_S32DS_3.4.3_D2205 SW32K3_S32DS_3.4.3_D2112.png

0 Kudos
Reply