Run code immediately on reset without starting debug (S32K116 evaluation board)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Run code immediately on reset without starting debug (S32K116 evaluation board)

1,700件の閲覧回数
Drifter22
Contributor II

Hi, my code on the evaluation board doesn't run when I power on the board (via OpenSDA on USB): I have to start debugging to run the code. How can I set the board to run the code always when powered (even with external power supply, without connecting to the USB)?

0 件の賞賛
返信
1 返信

1,688件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi,

Please make sure code is in the Flash not SRAM.

You can power the board via the 12V connector, you need to change J107 to position 1-2.

danielmartynek_0-1604046048473.png

 

Regards,

Daniel

 

0 件の賞賛
返信