Reset Generator question

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Reset Generator question

Jump to solution
1,097 Views
Febins
Contributor I

Hi there, I am trying to answer some question from my company, cannot seem to find the answer for it. We are using S32K118 .

question 1) 

What is the highest voltage that the reset generator tracks Vcc before becoming active (e.g. reset follows the Vcc rail until Vcc reaches 1V)?

Febins_0-1724100702488.png

 

question 2) Is the reset generator slew rate dependent (see figure in 3.2.105 above dv/dt)?  

It would be really helpful if someone can answer this,

thanks

 

0 Kudos
Reply
1 Solution
1,065 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @Febins,

1.

Out of the power-on reset, the MCU (its PN junctions) is not biased.

So, the reset module cannot control the reset_b until the VDD voltage reaches the forward bias voltage.

Once it can control the reset_b, the pin is asserted and stays asserted until the VDD LVR deassert level is reached.

2.

The ramp rate simply follows the VDD voltage.

 

Regards,

Daniel

 

View solution in original post

0 Kudos
Reply
3 Replies
1,066 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @Febins,

1.

Out of the power-on reset, the MCU (its PN junctions) is not biased.

So, the reset module cannot control the reset_b until the VDD voltage reaches the forward bias voltage.

Once it can control the reset_b, the pin is asserted and stays asserted until the VDD LVR deassert level is reached.

2.

The ramp rate simply follows the VDD voltage.

 

Regards,

Daniel

 

0 Kudos
Reply
988 Views
Febins
Contributor I
1. Can you tell me what is the voltage value of VDD LVR deasset level? thanks
0 Kudos
Reply
961 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @Febins,

There is the assert threshold and its hysteresis specified in the DS.

danielmartynek_0-1725216976623.png

 

BR, Daniel

 

0 Kudos
Reply