Regarding External Flash writing issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Regarding External Flash writing issue

1,437件の閲覧回数
Pragadeesh
Contributor I

Hi, 

 

I am using S32K342 variant chip , in that i want to write data in External flash through QSPI, for that I am using FLS module from the RTD package SW32K3_RTD_4.4_2.0.0 , actually i can able to erase , read and write, but writing is not happening the proper order, i can see the 1st 4 bytes of data is swapped to last of the initialized buffer, for more information i have attached the picture.

 

 

Thanks & Regards,

Pragadeesh

0 件の賞賛
返信
1 返信

1,424件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

Do you see this failure also over AHB read?

0 件の賞賛
返信