Read / Write gpio

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,879件の閲覧回数
Sanchita_Kochar
Contributor II

For S32K324,

how to write on gpio ?

how to read from gpio?

1 or 0, logic high or logic low

0 件の賞賛
返信
1 解決策
2,872件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

simple code using direct SIUL2 register

PetrS_0-1673006116471.png

If you would like to use RTD then refer to https://www.nxp.com/webapp/Download?colCode=06_S32K3XX_PINS_AND_CLOCKS_WITH_RTD_TRAINING and/or refer to e.g. Siul2_Dio_Ip_Example_S32K344 in the S32DS

BR, Petr

元の投稿で解決策を見る

2 返答(返信)
2,873件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

simple code using direct SIUL2 register

PetrS_0-1673006116471.png

If you would like to use RTD then refer to https://www.nxp.com/webapp/Download?colCode=06_S32K3XX_PINS_AND_CLOCKS_WITH_RTD_TRAINING and/or refer to e.g. Siul2_Dio_Ip_Example_S32K344 in the S32DS

BR, Petr

2,867件の閲覧回数
Sanchita_Kochar
Contributor II

Thank you so much!!!

0 件の賞賛
返信