S32K144 FTM Input capture Duty 0 -100%

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K144 FTM Input capture Duty 0 -100%

1,354 Views
enzofarneti
Contributor I

Hi,

I have configured FTM0 in Dual Edge Capture Mode in order to read frequency and duty cycle of an input signal.

All works fine if the duty cycle of input signal is >0% and <100%.

I'd like to understand how I can read 0% and 100% of duty --> Input signal  low or high DC.

Is it possible read input port also as GPIO (Digial Input) even this is configured  as FTM0 port?

Best Regards

0 Kudos
2 Replies

482 Views
JayFans302
Contributor I

How to mesure the frequency and duty cycle of an input signal at the same time in one project?Can you help me?Thanks!

0 Kudos

1,139 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi Enzo,

this was already discussed here:

https://community.nxp.com/thread/528539 

Regards,

Lukas

0 Kudos