RTD for s32k3 example project compilation error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

RTD for s32k3 example project compilation error

跳至解决方案
465 次查看
JhonYF
Contributor II

 

Using the example under the RTD path, I directly imported it into S32DS for compilation, but an error occurred. How should I handle this?

PATH:SW32K3_RTD_R21-11_4.0.0_HF_02\eclipse\plugins\Adc_TS_T40D34M40I0R0\examples\S32DS

JhonYF_0-1753770748308.png

 

 

 

0 项奖励
回复
1 解答
456 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

If you want to test the RTD examples in S32DS, please click: File ->  New -> S32DS Project from Example -> S32K3XX AUTOSAR R21-11 RTD 4.0.0 HF02 D2407 Example Projects -> Adc Examples ->

Then follow the description.txt of the example:
3.1 Generating the S32 configuration
Before running the example a configuration needs to be generated. First go to Project Explorer View in S32 DS and select the current project. Select the "S32 Configuration Tool" menu then click on the desired configuration tool (Pins, Cocks, Peripherals etc...).
Clicking on any one of those will generate all the components. Make the desired changes (if any) then click on the "S32 Configuration Tool->Update Code" button.


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

在原帖中查看解决方案

0 项奖励
回复
2 回复数
457 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

If you want to test the RTD examples in S32DS, please click: File ->  New -> S32DS Project from Example -> S32K3XX AUTOSAR R21-11 RTD 4.0.0 HF02 D2407 Example Projects -> Adc Examples ->

Then follow the description.txt of the example:
3.1 Generating the S32 configuration
Before running the example a configuration needs to be generated. First go to Project Explorer View in S32 DS and select the current project. Select the "S32 Configuration Tool" menu then click on the desired configuration tool (Pins, Cocks, Peripherals etc...).
Clicking on any one of those will generate all the components. Make the desired changes (if any) then click on the "S32 Configuration Tool->Update Code" button.


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

0 项奖励
回复
451 次查看
JhonYF
Contributor II
Thank you very much for your reply
0 项奖励
回复